This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWCAS-RF-EVM: 四片级联开发板通道相位一致性问题

Part Number: MMWCAS-RF-EVM


您好,

请问在使用MMWCAS-RF-EVM开发板时(MIMO方式),使用角反放在5m地方,分别采集-60°-60°的数据,分析发现不同发射、不同接收通道相位都偏差挺大的,如下图1为30°方向各通道相位曲线,横坐标为16个接收,同一个芯片的不同通道以及不同芯片的通道间都存在差异;

图1

图2为45°方向各通道相位曲线,也存在一定的相位波动,其他有些角度的波动会更大,拿0°方向做校准补偿同样存在不同通道间的差异,请问这个不同通道间相位一致性如何准确的去做对比分析,不同通道间的相位如何准确去做校准?

图2 

谢谢。