Other Parts Discussed in Thread: MMWAVEICBOOST,
您好!
使用IWR6843ISK + MMWAVEICBOOST烧写\mmwave_industrial_toolbox_4_9_0\labs\vital_signs\68xx_vital_signs\prebuilt_binaries\vital_signs_demo_68xx.bin,
修改功能模式后,可以使用VitalSignsRadar_Demo.exe测试呼吸和心跳。
但是修改IWR6843ISK的相关配置,单独使用该天线板,连接的是天线板的串口,会出现以下的报错:
QT version = 5.9.1
QMetaObject::connectSlotsByName: No matching signal for on_buttonBox_accepted()
Serial Port Found
Data Port Number is "COM7"
User Port Number is "COM7"
Data port succesfully Open
User port did not Open
用户说明中有:
The visualizer can only run with the following:
Industrial mmWave Carrier Board + IWR6843ISK Antenna Module
OR
+ IWR6843ISK-ODS Antenna Module
OR
+ IWR6843AOPEVM.
想咨询的是:这个例程是否不支持单独的IWR6843ISK天线板?