This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443: 有没有iwr1443 Rom BootLoder的程序流程图及运行参数表?

Part Number: IWR1443


IWR1443: iwr1443一上电,如何缩短将固件加载到RAM的时间? - 传感器论坛 - 传感器 - E2ETm 设计支持 (ti.com)

如该链接帖中提到,我想要缩短上电后Rom BootLoder将应用程序从Qspi Flash中读出到Program Ram的时间,由于Rom BootLoder不可更改,因此要自己开发SBL。

查看文档了解到,SBL是由Rom BootLoder从flash中读出到RAM,然后SBL开始运行去加载应用程序,那么Rom BootLoder中的Qspi读取速率是多少?另是以什么方式读取的呢(1bit/2bit/4bit的)??

假如bit rate设为40Mhz,dma方式quad读取,若没有SBL,Rom Bootloder加载110K代码,大概30ms,若有SBL,假如SBL 60KB,则这个时间由2部分构成,ROM Bootloder加载60KB SBL时间+SBL加载110KB应用程序时间,在SBL中可将bit rate设为最高60Mhz,这个时间未必会<30ms把??

请给出Rom BootLoder中的相关运行参数。