This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TDC1000: 器件的VCOM电压采用内置内部控制,正常是多少V的电压值?LNA放大器的输出没有输入波形的信息

Part Number: TDC1000


你好!我这边应用TDC1000时,碰到以下几个疑问:

1、VCOM的电压值正常应该是多少V,我用的是内部控制,在VCOM引脚上只有连接一个0.01uF的电容到地。通过示波器查看VCOM引脚的电压时发现,在TDC1000的引脚TX1上发送波形后,会抬高,大概在3V左右。维持340us左右又慢慢下降。通过改动配置参数,VCOM用内部产生和外部产生都一样的,如图1所示。1号的是TX1发送的波形,2号是VCOM的电压

2、采用信号发生器产生50KHz,1V Vpp,没有偏执电压,串个910欧姆电阻接到RX1引脚,LNA用电阻反馈,在LNAOUT引脚用示波器查看波形,在VCOM抬高的那个区间,没有发现信号发生器产生的波形信息。直接在PGAIN引脚输入该波形,在PGAOUT引脚用示波器看电压抬高区间也没有输入的波形信息。图2为信号发生器产生的信息,图3为RX1引脚的波形图,图4为LNAOUT引脚的波形图。

       

 3、TDC寄存器配置参数:TDC1000_reg_local_copy[10] = {0x49, 0x6B, 0x22, 0x48, 0x1F, 0xE4, 0x58, 0x01, 0x1A, 0x01};

希望哪个大神能够帮忙解决一下,不胜感激!