This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP126: 驱动程序

Part Number: TMP126


我写的TMP126驱动程序,希望TMP126单次转换执行后,读取一次结果,发现读取的温度转换值是  0x255,程序如下,帮忙看下是何原因?

#ifndef _TMP126_H
#define _TMP126_H

// TMP126的端口配置

#define TMP126_SCLK_OUT P1DIR|=BIT3
#define TMP126_SCLK_0 P1OUT&=~BIT3
#define TMP126_SCLK_1 P1OUT|=BIT3

#define TMP126_CS_OUT P3DIR|=BIT1
#define TMP126_CS_0 P3OUT&=~BIT1
#define TMP126_CS_1 P3OUT|=BIT1


#define TMP126_SIO_OUT P3DIR|=BIT0
#define TMP126_SIO_IN P3DIR&=~BIT0

#define TMP126_SO_0 P3OUT&=~BIT0
#define TMP126_SO_1 P3OUT|=BIT0

#define TMP126_SI_VAL ((P3IN&BIT0)==BIT0)

#define TMP126_DATAREG 0x00
#define TMP126_STATUS 0x02
#define TMP126_CONFIGREG 0x03


#define START_TMP126 0x01
#define WAIT_TMP126_CONVERT 0x02
#define READ_TMP126_RESULT 0x03
#define IDEL_TMP126 0x04

#define SET_TMP126_CONVERT 0x012 //one-slot,62.5ms/convter


unsigned char ReadTMP126Step;
unsigned char TMP126SleepFlag;


void TMP126_port_init(void);
void spi_write_int_to_TMP126(unsigned int x);
unsigned int spi_read_int_from_TMP126(void);
void write_TMP126_reg16(unsigned char reg,unsigned int data);
unsigned int read_TMP126_reg16(unsigned char reg);
void start_TMP126(void);
float read_temperature(void);

#endif

#include "all.h"


//******************************************************************************
// @brief :
// TMP126_port_init ioport direction & int
// @note:
// none
// @para:
// none
//******************************************************************************
void TMP126_port_init(void)
{
TMP126_SCLK_OUT;
TMP126_CS_OUT;
TMP126_SIO_OUT;

}

//******************************************************************************
// @brief :
// write a int data to TMP126
// @note:
// none
// @para:
// uint_16 x data
//******************************************************************************
void spi_write_int_to_TMP126(unsigned int x)
{
for(unsigned char i=0;i<16;i++)
{
TMP126_SCLK_0;

if((x&0x8000)==0x8000)
{
TMP126_SO_1;
}
else
{
TMP126_SO_0;
}
x<<=1;

TMP126_SCLK_1;

}

}

//******************************************************************************
// @brief :
// read a int data from TMP126
// @note:
// none
// @para:
// uint_16 x data
//******************************************************************************
unsigned int spi_read_int_from_TMP126(void)
{
unsigned char x;
TMP126_SIO_IN;
TMP126_SCLK_1;

for(unsigned char i=0;i<16;i++)
{
TMP126_SCLK_0;

x<<=1;
if(TMP126_SI_VAL)
{
x|=0x01;
}
else
{
x&=~0x01;
}
TMP126_SCLK_1;

}
return x;


}

void write_TMP126_reg16(unsigned char reg,unsigned int data)
{
unsigned int temp=0;
TMP126_SIO_OUT;
temp|=reg;
spi_write_int_to_TMP126(temp);
spi_write_int_to_TMP126(data);

TMP126_SO_1;
TMP126_SIO_OUT;

}
unsigned int read_TMP126_reg16(unsigned char reg)
{
unsigned int temp=0x100;
TMP126_SIO_OUT;
temp|=reg;
spi_write_int_to_TMP126(temp);
TMP126_SIO_IN;
temp=spi_read_int_from_TMP126();
return temp;

}

void start_TMP126(void)
{
TMP126_CS_0;
write_TMP126_reg16(TMP126_CONFIGREG,SET_TMP126_CONVERT);
TMP126_CS_1;
}


float read_temperature(void)
{
float f=-100;
unsigned int status;
INT16U x;

TMP126_CS_0;
status=read_TMP126_reg16(TMP126_STATUS);
TMP126_CS_1;

TMP126_CS_0;
x=read_TMP126_reg16(TMP126_DATAREG);
TMP126_CS_1;
if((status&BIT0)==BIT0)
{
f=(x)*0.0078125;// 0.0078125=0.03125/4
}

return f;

}