This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
在MATLAB上跑完TI给的例程(RSTD_Interface_Example)之后,mmwavesudio中Output界面已经出现了“Running Man script from MATLAB”。再用MATLAB指令运行mmwave_studio_02_01_01_00\mmWaveStudio\Scripts\Automation.lua.(已将Automation.lua中的串口号改为上位机串口号)mmwave Output界面出现“未将对象引用设置到对象的实例”。
以下为mmwave中output的输出结果和MATLAB代码。第一次在TI论坛交流,有表达不到位的,还望各位前辈指正。
%% RSTD_Interface_Example.m addpath(genpath('.\')) % Initialize mmWaveStudio .NET connection RSTD_DLL_Path = 'C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\Clients\RtttNetClientController\RtttNetClientAPI.dll'; ErrStatus = Init_RSTD_Connection(RSTD_DLL_Path); if (ErrStatus ~= 30000) disp('Error inside Init_RSTD_Connection'); return; end %Example Lua Command strFilename = 'C:\\ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\Scripts\\Automation_1.lua'; Lua_String = sprintf('dofile("%s")',strFilename); ErrStatus =RtttNetClientAPI.RtttNetClient.SendCommand(Lua_String); %% Init_RSTD_Connection.m function ErrStatus = Init_RSTD_Connection(RSTD_DLL_Path) %This script establishes the connection with mmWaveStudio software % Pre-requisites: % Type RSTD.NetStart() in mmWaveStudio Luashell before running the script. This would open port 2777 % Returns 30000 if no error. if (strcmp(which('RtttNetClientAPI.RtttNetClient.IsConnected'),'')) %First time the code is run after opening MATLAB disp('Adding RSTD Assembly'); RSTD_Assembly = NET.addAssembly(RSTD_DLL_Path); if ~strcmp(RSTD_Assembly.Classes{1},'RtttNetClientAPI.RtttClient') disp('RSTD Assembly not loaded correctly. Check DLL path'); ErrStatus = -10; return end Init_RSTD_Connection_1 = 1; elseif ~RtttNetClientAPI.RtttNetClient.IsConnected() %Not the first time but port is disconnected % Reason: % Init will reset the value of Isconnected. Hence Isconnected should be checked before Init % However, Isconnected returns null for the 1st time after opening MATLAB % (since init was never called before) Init_RSTD_Connection_1 = 1; else Init_RSTD_Connection_1 = 0; end if Init_RSTD_Connection_1 disp('Initializing RSTD client'); ErrStatus = RtttNetClientAPI.RtttNetClient.Init(); if (ErrStatus ~= 0) disp('Unable to initialize NetClient DLL'); return; end disp('Connecting to RSTD client'); ErrStatus = RtttNetClientAPI.RtttNetClient.Connect('127.0.0.1',2777); if(ErrStatus ~= 0) disp('Unable to connect to mmWaveStudio'); disp('Reopen port in mmWaveStudio. Type RSTD.NetClose() followed by RSTD.NetStart()'); return; end pause(1);%Wait for 1sec. NOT a MUST have. end disp('Sending test message to RSTD'); Lua_String = 'WriteToLog("Running script from MATLAB\n", "green")'; ErrStatus = RtttNetClientAPI.RtttNetClient.SendCommand(Lua_String); if (ErrStatus ~= 30000) disp('mmWaveStudio Connection Failed'); end disp('Test message success'); end
你好,
你能否下载一下mmwave studio 3.00.00.14?我尝试过下面的代码可以成功运行,你可以参考相关代码。
C:\ti\mmwave_studio_03_00_00_14\mmWaveStudio\MatlabExamples\4chip_cascade_TxBF_example\cascade_TxBF_dataCapture.m