This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: mmwavelinxk_example.exe 配置修改,实现3发4收TMD-MIMO中的chirp配置和frame配置问题?

Part Number: AWR2243


您好,我在使用mmwave_dfp_02_02_03_01中的示例程序mmWaveLink_SingleChip_Example遇到一些问题:

我希望配置雷达为3发4收TMD-MIMO雷达,因此我配置了3个chirp,然后配置帧使用这3个chirp,相关配置如下:

#Chirp Configuration parameters, please modify if needed.
#rlChirpCfg_t
#
chirpStartIdx=0;
chirpEndIdx=0;
profileIdCPCFG=0;
startFreqVar=0;
freqSlopeVar=0;
idleTimeVar=0;
adcStartTimeVar=0;
txEnable=1;
#END

#
#Chirp Configuration parameters, please modify if needed.
#rlChirpCfg_t
#
chirpStartIdx=1;
chirpEndIdx=1;
profileIdCPCFG=0;
startFreqVar=0;
freqSlopeVar=0;
idleTimeVar=0;
adcStartTimeVar=0;
txEnable=2;
#END

#
#Chirp Configuration parameters, please modify if needed.
#rlChirpCfg_t
#
chirpStartIdx=2;
chirpEndIdx=2;
profileIdCPCFG=0;
startFreqVar=0;
freqSlopeVar=0;
idleTimeVar=0;
adcStartTimeVar=0;
txEnable=4;
#END

#
#Frame configuration parameters, please modify if needed.
#rlFrameCfg_t
#
chirpStartIdxFCF=0;
chirpEndIdxFCF=2;
frameCount=320;
loopCount=64;
periodicity=20000000;
triggerDelay=0;
numAdcSamples=512;
triggerSelect=1;
#END

但是运行mmwavelinxk_example.exe出现如下错误:

(1)

(2) 

第一处错误,并没有导致程序终止,但是在mmwaveconfig.txt中我明明配置了3个chirp,这里只执行了两次 rlSetChirpConfig?

第二处错误导致程序终止,请问我应该怎么修改配置文件解决这两个错误?

另外请问有3发4收的雷达示例配置可以参考么,dfp中的示例程序似乎都是2发4收的?

  • 第一处错误,并没有导致程序终止

    请根据错误信息,在代码debug一下错误原因。

    但是在mmwaveconfig.txt中我明明配置了3个chirp,这里只执行了两次 rlSetChirpConfig?

    请在代码中添加打印看看为什么只调用了两次。

  • 您好,问题已经解决

    通过阅读代码,我发现确实是代码中存在bug,示例中写的代码只支持2TX

    int MMWL_chirpConfig(unsigned char deviceMap)
    {
        int i, retVal = RL_RET_CODE_OK;
    	rlChirpCfg_t setChirpCfgArgs[2] = { 0 };
    
        rlChirpCfg_t getChirpCfgArgs[MAX_GET_CHIRP_CONFIG_IDX+1] = {0};
    
        /*read chirpCfgArgs from config file*/
        MMWL_readChirpConfig(&setChirpCfgArgs[0], 2);
    
        printf("Calling rlSetChirpConfig with \nProfileId[%d]\nStart Idx[%d]\nEnd Idx[%d] \n\n",
                    setChirpCfgArgs[0].profileId, setChirpCfgArgs[0].chirpStartIdx,
                    setChirpCfgArgs[0].chirpEndIdx);
    
    	printf("Calling rlSetChirpConfig with \nProfileId[%d]\nStart Idx[%d]\nEnd Idx[%d] \n\n",
    		setChirpCfgArgs[1].profileId, setChirpCfgArgs[1].chirpStartIdx,
    		setChirpCfgArgs[1].chirpEndIdx);
    
        /* With this API we can configure max 512 chirp in one call */
        retVal = rlSetChirpConfig(deviceMap, 2U, &setChirpCfgArgs[0U]);
    
        /* read back Chirp config, to verify that setChirpConfig actually set to Device
          @Note - This examples read back (10+1) num of chirp config for demonstration,
                   which user can raise to match with their requirement */
        retVal = rlGetChirpConfig(deviceMap, setChirpCfgArgs[0].chirpStartIdx,
                                  setChirpCfgArgs[0].chirpStartIdx + MAX_GET_CHIRP_CONFIG_IDX, &getChirpCfgArgs[0]);
        if (retVal != RL_RET_CODE_OK)
        {
            printf("GetChirp Configuration failed for deviceMap %u with error %d \n\n",
                    deviceMap, retVal);
        }
        else
        {
            for (i=0; i <= MAX_GET_CHIRP_CONFIG_IDX; i++)
            {
                /* @Note- This check assumes that all chirp configs are configured by single setChirpCfgArgs[0] */
                /* compare each chirpConfig parameters to lastly configured via rlDynChirpConfig API 
    			*/
                if ((getChirpCfgArgs[i].profileId != setChirpCfgArgs[0].profileId) || \
                    (getChirpCfgArgs[i].freqSlopeVar != setChirpCfgArgs[0].freqSlopeVar) || \
                    (getChirpCfgArgs[i].txEnable != setChirpCfgArgs[0].txEnable) || \
                    (getChirpCfgArgs[i].startFreqVar != setChirpCfgArgs[0].startFreqVar) || \
                    (getChirpCfgArgs[i].idleTimeVar != setChirpCfgArgs[0].idleTimeVar) || \
                    (getChirpCfgArgs[i].adcStartTimeVar != setChirpCfgArgs[0].adcStartTimeVar))
                {
                    printf("*** Failed - Parameters are mismatched GetChirpConfig compare to rlSetChirpConfig *** \n\n");
                    break;
                }
    
            }
    
            if (i > MAX_GET_CHIRP_CONFIG_IDX)
            {
                printf("Get chirp configurations are matching with parameters configured during rlSetChirpConfig \n\n");
            }
        }
    
        return retVal;
    }

    修改代码中第四行为

    rlChirpCfg_t setChirpCfgArgs[3] = { 0 };

    第20行为:

    retVal = rlSetChirpConfig(deviceMap, 3U, &setChirpCfgArgs[0U]);

    代码已经可以正常运行,