This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843: Calculate the slope of chirp according to the maximum distance and if bandwidth

Part Number: AWR1843

Hi,expert

In the following documents,

there are the following descriptions(page 7):

IFmax=10MHz,dmax=150m,S=4MHz/us,

However,according to the formula,dmax=IF*c/(2*S),S=10MHz/us.

Why are the results in the document different from the actual calculation results?