您好,我想教教几个问题。如果我有2部雷达:AWR1843。我想让他们放置在不同位置对同一个运动目标进行检测实现双基地雷达(一部雷达只是发射信号,另一部雷达只是接收信号)。我注意到了这篇文章:AWR1443BOOST: Realization of SPI control using two AWR1443BOOST - Sensors forum - Sensors - TI E2E support forums
1.如果我要实现只用一台电脑接收数据对于AWR1843来说应该和他一样的设置吗?
2.我之前没有用MSS编写源码的基础,只是用过软件界面设置参数,如何快速的实现这样的配置实现一部雷达发射另一部雷达接收的这种情况呢?
3.能否提供详细的步骤呢?
4.这种设置后,我要调整参数还是通过电脑上的GUI界面勾选参数吗?
非常感谢
请工程师解答一下!万分感谢