This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
这个问题已经困扰我好几天了,查找资料无果,程序烧写成功后,运行GUI 端口 user port did not open 需要怎么处理?
另外就是烧写程序时候 成功次数只有偶然 请问具体应该如何烧写?
我是用Uniflash烧写
1. uniflash烧写可以看一下下面的视频。
https://training.ti.com/hardware-setup-iwr6843isk-and-iwr6843isk-ods
不稳定的话,看一下供电电源是否5V, 3A
2. 运行vital sign demo需要MMWAVEICBOOST 板子+mmwave antenna board。请问有使用MMWAVEICBOOST板子么?
The visualizer can only run with the following:
Industrial mmWave Carrier Board + IWR6843ISK Antenna Module
OR
+ IWR6843ISK-ODS Antenna Module
OR
+ IWR6843AOPEVM.
https://dev.ti.com/tirex/explore/node?node=ADTLXelX36I6iOJjRnxYYA__VLyFKFf__LATEST
抱歉,文档里的GUI没有公开。
请尝试使用matlab版本的GUI,C:\ti\mmwave_industrial_toolbox_4_9_0\labs\vital_signs\14xx_vital_signs\gui,这个GUI不识别XDS110的串口。