This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOPEVM: 能否用DSP控制HWA

Part Number: IWR6843AOPEVM


在68xx系列的demo中,HWA好像都是用ARM控制的。我想问一下能否用DSP控制HWA?68系列是否有使用DSP控制HWA的demo?

  • HWA主要通过硬件做radar FMCW算法方面的处理,分担DSP的一些算法,可以和DSP同时运行。两者可以传递数据。请看下面的HWA文档说明。
    Alternately, if the ADC output samples are required to be pre-processed by the DSP before processing by the Hardware Accelerator, then the ADC buffer sharing can be disabled (see the FFT1DEN register bit), such that the DSP can access the ADC buffer, perform the pre-processing as needed, and then write to the dedicated local memories (ACCEL_MEM0 and ACCEL_MEM1) of the Radar Hardware Accelerator for further processing using the accelerator.
    https://www.ti.com/lit/ug/swru526b/swru526b.pdf

    一般情况下,HWA处理好数据后就由ARM核去发送了,我们没有DSP控制HWA的demo。

  • 我们打算在HWA上进行2D-FFT,DSP上的神经网络处理HWA的2D-FFT结果,然后ARM将DSP上神经网络的处理结果发给电脑。请问此种情况下有无必要使用DSP控制HWA?

  • 可以把HWA处理的数据发给DSP,可以看一下HWA的数据输入输出框图。
    Figure 3. Hardware Accelerator Block Diagram
    https://www.ti.com/lit/an/swra621/swra621.pdf