我看到对于级联板的手册中提到在每次采集中第一帧会被干扰,所以建议忽略,那么级联板输出的bin文件是已经忽略第一帧后的结果还是需要我自己进行处理,因为我在测试的时候发现如果我如下配置:
16位复采样
256采样点
12个Chirp
64个Loop
8帧
我应该得到的每一个芯片的数据是2*2*4*256*12*64*8/1024/1024=24MB,但是我实际拿到的每个bin文件的输出是21MB
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请看mmwave_studio_release_notes.pdf里的limitation。
- The first frame may be corrupted in every capture. It is recommended to ignore the first frame for all captures.
- Also, the number of frames captured by the TDA2 is one less than the number of frames sent by the AWR devices when the AWR devices are configured to send out a finite number of frames