This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: 信号传输问题

Part Number: AWR1642BOOST


我在DSS中有一个变量,然后我在mss中使用WritePolling函数进行输出,build提示我这个变量未定义,我的猜测是我没有把这个变量传输到MSS中。截图如下

我有3个问题。第一个是:我该如何将解决这个错误,我该如何把这个变量传输过去?

第二个是:我这个WritePolling函数是在mss_main.c中的static void MmwDemo_mboxReadTask这个函数中调用的,我想知道他是将数据通过XDS110串口输出出去了吗?

第三个:我的功能实现需要把这个变量输出到外部的单片机,所以需要连接RS232的线,我想知道我定义的的时候是通过这些代码进行编辑码?