This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: AWR2243 cascade 20 GHz LO Distribution

Part Number: AWR2243


各位Ti的工程师,

我们现在重新设计了级联方案的RF板,重新分配了Master IC的20 GHz LO Distribution信号,

Demo RF板:

1、OUT D1(FM_CW_SYNCOUT) 

2、IN B1(FM_CW_SYNCIN1)

3、OUT B15(FM_CW_CLKOUT)

当前设计RF板:

1、OUT D1(FM_CW_SYNCOUT)

2、IN D15(FM_CW_SYNCIN2)

3、OUT B15(FM_CW_CLKOUT)

这样跟级联方案的Host Demo板匹配使用,可以直接使用吗,还是需要通过TDA2重新配置?

谢谢。