This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWCAS-DSP-EVM: MMWCAS-DSP-EVM:

Part Number: MMWCAS-DSP-EVM


增加一个关联的问题:是否需要先给FPGA烧录程序后 TDA2才能进入SD卡BOOT 模式。

目前遇到FPGA未烧录,TDA2模式已选择SD卡模式,上电后,TDA2的 SMDCLK 没有波形输出。

  • 能否提供一下 TDA2S 烧录相关资料文档

  • 你好,

    MMWCAS-DSP-EVM上的FPGA在出厂前是烧写好的,用户是不需烧写的。

    如果你使用的是自己参考MMWCAS-DSP-EVM做的板子,理论上TDA2的启动时和芯片的boot mode设置相关,在TDA芯片reset信号从低变高前去读取boot mode信息,rom code会根据boot mode的配置运行相关的启动流程。你可以关注一下相关引脚在TDA芯片reset信号从低变高时候的电平。

    关于TDA2启动,你可以参考TDA2 TRM里Initialization章节的内容。

  • 芯片的boot mode设置从SD卡启动,上电后,TDA2的 SMDCLK 输出方波(TDA2进入启动流程),插入Boot SD 卡,SMDCLK置低。RESET  TDA2,SMDCLK 输出一段方波后,置低,没有加载SD卡内的数据。

    这样是Boot 失败吗? 串口没无法输入TDA2的状态日志,有什么方式可以查看?

  • Jack,

    启动的SD卡需要在上电前就插入的啊,第一个启动设备/方法失败后,会继续后面的启动方式。下面的信息可以在TDA2 TRM里找到。

  • Hi,Chris,Boot配置如下图.  上电之前接入SD卡,现象一致,SDCLK 有一段波形后,持续置低了。 测试到BOOT 11 引脚会持续置高

  • 你好,

    请问你板上有仿真器接口么?能否连上仿真器看看CTRL_CORE_BOOTSTRAP寄存器的值,里面可以了解上电复位时候芯片读取的sysboot信号的值。你可以对比看看和你预想的是否一致。

    请问在这张启动的SD卡是否有在TI的EVM上测试过是可以正常启动的?

  • 你好,

    请问你这块FPGA没有代码的板子和MMWCAS-DSP-EVM一模一样么?还是有删减?在MMWCAS-DSP-EVM里U62这个选择开关以及相关电路是否有保留?

  • 有删减DDR电路 只保留: DDR3-1066  32-Bit+ECC EMIF1 (2x Micron MT41K512M16HA-125)

    SD卡在TI的EVM上测试过是可以正常启动,log如下。U62这个选择开关以及相关电路保留。

    U-Boot SPL 2016.05-00018-g6bc25a5 (Aug 05 2019 - 14:43:03)
    DRA752-GP ES2.0
    no pinctrl for hs200_1_8v
    no pinctrl for ddr_1_8v
    Card did not respond to voltage select!
    *** Warning - MMC init failed, using default environment
    
    Trying to boot from MMC1
    reading dra7-ipu2-fw.lzop
    spl_load_file_fat: error reading file dra7-ipu2-fw.lzop, err - -1
    spl: error reading image dra7-ipu2-fw.lzop, err - -1
    Error loading remotecore IPU2!,Continuing with boot ...
    reading dra7-dsp1-fw.lzop
    spl_load_file_fat: error reading file dra7-dsp1-fw.lzop, err - -1
    spl: error reading image dra7-dsp1-fw.lzop, err - -1
    Error loading remotecore DSP1!,Continuing with boot ...
    reading dra7-dsp2-fw.lzop
    spl_load_file_fat: error reading file dra7-dsp2-fw.lzop, err - -1
    spl: error reading image dra7-dsp2-fw.lzop, err - -1
    Error loading remotecore DSP2!,Continuing with boot ...
    reading dra7-ipu1-fw.lzop
    spl_load_file_fat: error reading file dra7-ipu1-fw.lzop, err - -1
    spl: error reading image dra7-ipu1-fw.lzop, err - -1
    Error loading remotecore IPU1!,Continuing with boot ...
    spl: falcon_args_file not set in environment, falling back to default
    reading single-stage-boot.dtb
    spl_load_image_fat_os: error reading image single-stage-boot.dtb, err - -1
    reading u-boot.img
    reading u-boot.img
    reading u-boot.img
    reading u-boot.img
    
    
    U-Boot 2016.05-00018-g6bc25a5 (Aug 05 2019 - 14:43:03 +0530)
    
    CPU  : DRA752-GP ES2.0
    Model: TI DRA742
    Board: DRA74x Cascade EVM REV H.4
    DRAM:  4 GiB
    MMC:   i2c_write: error waiting for data ACK (status=0x116)
    pcf8575_i2c_write_le16 i2c write failed to addr 21
    OMAP SD/MMC: 0, OMAP SD/MMC: 1
    Card did not respond to voltage select!
    *** Warning - MMC init failed, using default environment
    
    Card did not respond to voltage select!
    ERROR: invalid mmc device
    
    at arch/arm/cpu/armv7/omap-common/utils.c:193/mmc_get_part_size()
    Warning: fastboot.userdata_size: unable to calc
    SCSI:  SATA link 0 timeout.
    AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl SATA mode
    flags: 64bit ncq stag pm led clo only pmp pio slum part ccc apst 
    scanning bus for devices...
    Found 0 device(s).
    Net:   Could not get PHY for ethernet@48484000: addr 2
    
    Warning: ethernet@48484000 using MAC address from ROM
    eth0: ethernet@48484000
    Hit any key to stop autoboot:  2  1  0 
    ## Error: "board_findfdt" not defined
    i2c_write: error waiting for data ACK (status=0x116)
    pcf8575_i2c_write_le16 i2c write failed to addr 21
    i2c_write: error waiting for data ACK (status=0x116)
    pcf8575_i2c_write_le16 i2c write failed to addr 21
    switch to partitions #0, OK
    mmc0 is current device
    i2c_write: error waiting for data ACK (status=0x116)
    pcf8575_i2c_write_le16 i2c write failed to addr 21
    i2c_write: error waiting for data ACK (status=0x116)
    pcf8575_i2c_write_le16 i2c write failed to addr 21
    SD/MMC found on device 0
    reading boot.scr
    ** Unable to read file boot.scr **
    reading uEnv.txt
    185 bytes read in 3 ms (59.6 KiB/s)
    Loaded env from uEnv.txt
    Importing environment from mmc0 ...
    i2c_write: error waiting for data ACK (status=0x116)
    pcf8575_i2c_write_le16 i2c write failed to addr 21
    i2c_write: error waiting for data ACK (status=0x116)
    pcf8575_i2c_write_le16 i2c write failed to addr 21
    switch to partitions #0, OK
    mmc0 is current device
    i2c_write: error waiting for data ACK (status=0x116)
    pcf8575_i2c_write_le16 i2c write failed to addr 21
    i2c_write: error waiting for data ACK (status=0x116)
    pcf8575_i2c_write_le16 i2c write failed to addr 21
    SD/MMC found on device 0
    3577032 bytes read in 171 ms (19.9 MiB/s)
    107792 bytes read in 25 ms (4.1 MiB/s)
    Booting from mmc0 ...
    Kernel image @ 0x82000000 [ 0x000000 - 0x3694c8 ]
    ## Flattened Device Tree blob at 88000000
       Booting using the fdt blob at 0x88000000
       Loading Device Tree to 8ffe2000, end 8ffff50f ... OK
    
    Starting kernel ...
    
    [    0.000000] Booting Linux on physical CPU 0x0
    [    0.000000] Initializing cgroup subsys cpuset
    [    0.000000] Initializing cgroup subsys cpu
    [    0.000000] Initializing cgroup subsys cpuacct
    [    0.000000] Linux version 4.4.84-00041-g84382ab (x0284921@bangvideoapps02) (gcc version 5.3.1 20160113 (Linaro GCC 5.3-2016.02) ) #1 SMP PREEMPT Mon Aug 5 14:52:40 IST 2019
    [    0.000000] CPU: ARMv7 Processor [412fc0f2] revision 2 (ARMv7), cr=30c5387d
    [    0.000000] CPU: PIPT / VIPT nonaliasing data cache, PIPT instruction cache
    [    0.000000] Machine model: TI DRA742 Cascade Radar Board
    [    0.000000] Reserved memory: created DMA memory pool at 0x0000000040300000, size 3 MiB
    [    0.000000] Reserved memory: initialized node cmem@40300000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: regions without no-map are not yet supported
    [    0.000000] Reserved memory: created CMA memory pool at 0x0000000099000000, size 80 MiB
    [    0.000000] Reserved memory: initialized node ipu2_cma@95800000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created CMA memory pool at 0x000000009e000000, size 32 MiB
    [    0.000000] Reserved memory: initialized node ipu1_cma@9d000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: regions without no-map are not yet supported
    [    0.000000] Reserved memory: created CMA memory pool at 0x00000000a1000000, size 32 MiB
    [    0.000000] Reserved memory: initialized node dsp1_cma@99000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: created CMA memory pool at 0x00000000a3000000, size 32 MiB
    [    0.000000] Reserved memory: initialized node dsp2_cma@9f000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: regions without no-map are not yet supported
    [    0.000000] Reserved memory: created DMA memory pool at 0x00000000a9000000, size 64 MiB
    [    0.000000] Reserved memory: initialized node cmem@A9000000, compatible id shared-dma-pool
    [    0.000000] Reserved memory: regions without no-map are not yet supported
    [    0.000000] cma: Reserved 64 MiB at 0x00000000bc000000
    [    0.000000] Forcing write-allocate cache policy for SMP
    [    0.000000] Memory policy: Data cache writealloc
    [    0.000000] OMAP4: Map 0x000000027fd00000 to fe600000 for dram barrier
    [    0.000000] DRA752 ES2.0
    [    0.000000] PERCPU: Embedded 11 pages/cpu @f2f1e000 s14912 r8192 d21952 u45056
    [    0.000000] Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 1025330
    [    0.000000] Kernel command line: console=ttyO0,115200n8 vram=16M root=PARTUUID=3cc717e1-02 rw rootwait ip=none cma=64M vmalloc=128M
    [    0.000000] PID hash table entries: 4096 (order: 2, 16384 bytes)
    [    0.000000] Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)
    [    0.000000] Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)
    [    0.000000] Memory: 2439424K/4109312K available (6671K kernel code, 320K rwdata, 2396K rodata, 336K init, 290K bss, 1424128K reserved, 245760K cma-reserved, 2167808K highmem)
    [    0.000000] Virtual kernel memory layout:
    [    0.000000]     vector  : 0xffff0000 - 0xffff1000   (   4 kB)
    [    0.000000]     fixmap  : 0xffc00000 - 0xfff00000   (3072 kB)
    [    0.000000]     vmalloc : 0xf8000000 - 0xff800000   ( 120 MB)
    [    0.000000]     lowmem  : 0xc0000000 - 0xf7800000   ( 888 MB)
    [    0.000000]     pkmap   : 0xbfe00000 - 0xc0000000   (   2 MB)
    [    0.000000]     modules : 0xbf000000 - 0xbfe00000   (  14 MB)
    [    0.000000]       .text : 0xc0008000 - 0xc08e302c   (9069 kB)
    [    0.000000]       .init : 0xc08e4000 - 0xc0938000   ( 336 kB)
    [    0.000000]       .data : 0xc0938000 - 0xc0988220   ( 321 kB)
    [    0.000000]        .bss : 0xc098a000 - 0xc09d2880   ( 291 kB)
    [    0.000000] SLUB: HWalign=64, Order=0-3, MinObjects=0, CPUs=2, Nodes=1
    [    0.000000] Preemptible hierarchical RCU implementation.
    [    0.000000] 	Build-time adjustment of leaf fanout to 32.
    [    0.000000] NR_IRQS:16 nr_irqs:16 16
    [    0.000000] ti_dt_clocks_register: failed to lookup clock node gmac_gmii_ref_clk_div
    [    0.000000] OMAP clockevent source: timer1 at 32786 Hz
    [    0.000000] Architected cp15 timer(s) running at 6.14MHz (phys).
    [    0.000000] clocksource: arch_sys_counter: mask: 0xffffffffffffff max_cycles: 0x16af5adb9, max_idle_ns: 440795202250 ns
    [    0.000005] sched_clock: 56 bits at 6MHz, resolution 162ns, wraps every 4398046511023ns
    [    0.000016] Switching to timer-based delay loop, resolution 162ns
    [    0.000332] clocksource: 32k_counter: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 58327039986419 ns
    [    0.000340] OMAP clocksource: 32k_counter at 32768 Hz
    [    0.000785] Console: colour dummy device 80x30
    [    0.000801] WARNING: Your 'console=ttyO0' has been replaced by 'ttyS0'
    [    0.000808] This ensures that you still see kernel messages. Please
    [    0.000813] update your kernel commandline.
    [    0.000826] Calibrating delay loop (skipped), value calculated using timer frequency.. 12.29 BogoMIPS (lpj=61475)
    [    0.000839] pid_max: default: 32768 minimum: 301
    [    0.000938] Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)
    [    0.000948] Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)
    [    0.001493] Initializing cgroup subsys io
    [    0.001509] Initializing cgroup subsys memory
    [    0.001533] Initializing cgroup subsys devices
    [    0.001546] Initializing cgroup subsys freezer
    [    0.001557] Initializing cgroup subsys perf_event
    [    0.001568] Initializing cgroup subsys pids
    [    0.001595] CPU: Testing write buffer coherency: ok
    [    0.001793] /cpus/cpu@0 missing clock-frequency property
    [    0.001809] /cpus/cpu@1 missing clock-frequency property
    [    0.001820] CPU0: thread -1, cpu 0, socket 0, mpidr 80000000
    [    0.001853] Setting up static identity map for 0x80008380 - 0x800083e0
    [    0.080055] CPU1: thread -1, cpu 1, socket 0, mpidr 80000001
    [    0.080126] Brought up 2 CPUs
    [    0.080139] SMP: Total of 2 processors activated (24.59 BogoMIPS).
    [    0.080145] CPU: All CPU(s) started in HYP mode.
    [    0.080150] CPU: Virtualization extensions available.
    [    0.080528] devtmpfs: initialized
    [    0.109542] VFP support v0.3: implementor 41 architecture 4 part 30 variant f rev 0
    [    0.110518] omap_hwmod: l3_main_2 using broken dt data from ocp
    [    0.314192] clocksource: jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 19112604462750000 ns
    [    0.314214] futex hash table entries: 512 (order: 3, 32768 bytes)
    [    0.319166] pinctrl core: initialized pinctrl subsystem
    [    0.320043] NET: Registered protocol family 16
    [    0.321012] DMA: preallocated 256 KiB pool for atomic coherent allocations
    [    0.350242] cpuidle: using governor ladder
    [    0.380268] cpuidle: using governor menu
    [    0.388798] OMAP GPIO hardware version 0.1
    [    0.392740] irq: no irq domain found for /ocp/l4@4a000000/scm@2000/pinmux@1400 !
    [    0.408134] omap-gpmc 50000000.gpmc: GPMC revision 6.0
    [    0.408147] gpmc_mem_init: disabling cs 0 mapped at 0x0-0x1000000
    [    0.417228] hw-breakpoint: found 5 (+1 reserved) breakpoint and 4 watchpoint registers.
    [    0.417238] hw-breakpoint: maximum watchpoint size is 8 bytes.
    [    0.417710] omap4_sram_init:Unable to allocate sram needed to handle errata I688
    [    0.417719] omap4_sram_init:Unable to get sram pool needed to handle errata I688
    [    0.418289] OMAP DMA hardware revision 0.0
    [    0.461509] omap-dma-engine 4a056000.dma-controller: OMAP DMA engine driver (LinkedList1/2/3 supported)
    [    0.462643] edma 43300000.edma: memcpy is disabled
    [    0.467331] edma 43300000.edma: TI EDMA DMA engine driver
    [    0.471420] omap-iommu 40d01000.mmu: 40d01000.mmu registered
    [    0.471603] omap-iommu 40d02000.mmu: 40d02000.mmu registered
    [    0.471761] omap-iommu 58882000.mmu: 58882000.mmu registered
    [    0.471920] omap-iommu 55082000.mmu: 55082000.mmu registered
    [    0.472196] omap-iommu 41501000.mmu: 41501000.mmu registered
    [    0.472399] omap-iommu 41502000.mmu: 41502000.mmu registered
    [    0.475436] palmas 0-0058: IRQ missing: skipping irq request
    [    0.490874] palmas 0-0058: Muxing GPIO 2e, PWM 0, LED 0
    [    0.552763] pcf857x: probe of 0-0020 failed with error -121
    [    0.553014] pcf857x: probe of 0-0021 failed with error -121
    [    0.553872] omap_i2c 48070000.i2c: bus 0 rev0.12 at 400 kHz
    [    0.554285] omap_i2c 48060000.i2c: bus 2 rev0.12 at 400 kHz
    [    0.554483] media: Linux media interface: v0.10
    [    0.554536] Linux video capture interface: v2.00
    [    0.554577] pps_core: LinuxPPS API ver. 1 registered
    [    0.554584] pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti <giometti@linux.it>
    [    0.554612] PTP clock support registered
    [    0.554661] EDAC MC: Ver: 3.0.0
    [    0.555413] omap-mailbox 48840000.mailbox: omap mailbox rev 0x400
    [    0.555702] omap-mailbox 48842000.mailbox: omap mailbox rev 0x400
    [    0.556031] Advanced Linux Sound Architecture Driver Initialized.
    [    0.556893] clocksource: Switched to clocksource arch_sys_counter
    [    0.567480] NET: Registered protocol family 2
    [    0.567989] TCP established hash table entries: 8192 (order: 3, 32768 bytes)
    [    0.568052] TCP bind hash table entries: 8192 (order: 4, 65536 bytes)
    [    0.568176] TCP: Hash tables configured (established 8192 bind 8192)
    [    0.568225] UDP hash table entries: 512 (order: 2, 16384 bytes)
    [    0.568256] UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)
    [    0.568399] NET: Registered protocol family 1
    [    0.568711] RPC: Registered named UNIX socket transport module.
    [    0.568721] RPC: Registered udp transport module.
    [    0.568727] RPC: Registered tcp transport module.
    [    0.568734] RPC: Registered tcp NFSv4.1 backchannel transport module.
    [    0.569699] hw perfevents: enabled with armv7_cortex_a15 PMU driver, 7 counters available
    [    0.579714] squashfs: version 4.0 (2009/01/31) Phillip Lougher
    [    0.580363] NFS: Registering the id_resolver key type
    [    0.580395] Key type id_resolver registered
    [    0.580403] Key type id_legacy registered
    [    0.580460] ntfs: driver 2.1.32 [Flags: R/O].
    [    0.581716] bounce: pool size: 64 pages
    [    0.581875] Block layer SCSI generic (bsg) driver version 0.4 loaded (major 247)
    [    0.581891] io scheduler noop registered
    [    0.581904] io scheduler deadline registered
    [    0.581938] io scheduler cfq registered (default)
    [    0.587425] pinctrl-single 4a003400.pinmux: 282 pins at pa fc003400 size 1128
    [    0.590956] PCI host bridge /ocp/axi@0/pcie_rc@51000000 ranges:
    [    0.590969]   No bus range found for /ocp/axi@0/pcie_rc@51000000, using [bus 00-ff]
    [    0.591002]    IO 0x20003000..0x20012fff -> 0x00000000
    [    0.591023]   MEM 0x20013000..0x2fffffff -> 0x20013000
    [    0.591234] dra7-pcie 51000000.pcie_rc: CFG 'Bus Master Enable' change
    [    0.591245] dra7-pcie 51000000.pcie_rc: CFG 'Memory Space Enable' change
    [    0.614751] dra7-pcie 51000000.pcie_rc: PCI host bridge to bus 0000:00
    [    0.614764] pci_bus 0000:00: root bus resource [bus 00-ff]
    [    0.614774] pci_bus 0000:00: root bus resource [io  0x0000-0xffff]
    [    0.614784] pci_bus 0000:00: root bus resource [mem 0x20013000-0x2fffffff]
    [    0.614847] dra7-pcie 51000000.pcie_rc: CFG 'Memory Space Enable' change
    [    0.614864] dra7-pcie 51000000.pcie_rc: CFG 'Memory Space Enable' change
    [    0.614890] dra7-pcie 51000000.pcie_rc: CFG 'Memory Space Enable' change
    [    0.614905] dra7-pcie 51000000.pcie_rc: CFG 'Memory Space Enable' change
    [    0.614926] dra7-pcie 51000000.pcie_rc: CFG 'Memory Space Enable' change
    [    0.614940] dra7-pcie 51000000.pcie_rc: CFG 'Memory Space Enable' change
    [    0.615242] PCI: bus0: Fast back to back transfers disabled
    [    0.626986] PCI: bus1: Fast back to back transfers disabled
    [    0.627115] pci 0000:00:00.0: BAR 0: assigned [mem 0x20100000-0x201fffff]
    [    0.627131] pci 0000:00:00.0: BAR 8: assigned [mem 0x20200000-0x202fffff]
    [    0.627142] pci 0000:00:00.0: BAR 1: assigned [mem 0x20020000-0x2002ffff]
    [    0.627157] pci 0000:01:00.0: BAR 0: assigned [mem 0x20200000-0x20203fff 64bit]
    [    0.627205] pci 0000:00:00.0: PCI bridge to [bus 01]
    [    0.627217] pci 0000:00:00.0:   bridge window [mem 0x20200000-0x202fffff]
    [    0.627429] pcieport 0000:00:00.0: Signaling PME through PCIe PME interrupt
    [    0.627438] pci 0000:01:00.0: Signaling PME through PCIe PME interrupt
    [    0.688532] Serial: 8250/16550 driver, 10 ports, IRQ sharing disabled
    [    0.691908] 4806a000.serial: ttyS0 at MMIO 0x4806a000 (irq = 202, base_baud = 3000000) is a 8250
    [    1.791843] console [ttyS0] enabled
    [    1.796236] 4806c000.serial: ttyS1 at MMIO 0x4806c000 (irq = 203, base_baud = 3000000) is a 8250
    [    1.805944] 48020000.serial: ttyS2 at MMIO 0x48020000 (irq = 204, base_baud = 3000000) is a 8250
    [    1.815963] [drm] Initialized drm 1.1.0 20060810
    [    1.821520] [drm] Supports vblank timestamp caching Rev 2 (21.10.2013).
    [    1.828207] [drm] No driver support for vblank timestamp query.
    [    1.834335] [drm] Initialized vdrm 1.0.0 20110917 on minor 0
    [    1.841482] OMAP DSS rev 6.1
    [    1.845229] omapdss_dss 58000000.dss: bound 58001000.dispc (ops dispc_component_ops)
    [    1.860816] loop: module loaded
    [    1.864354] vmemexp device MAJOR num = 245
    [    1.868507] vmemexp class registered
    [    1.872221] /dev/vmemexp device registered
    [    1.876336] ioctl DBUFIOC_EXPORT_VIRTMEM = -1072899120
    [    1.881883] nvme 0000:01:00.0: enabling device (0140 -> 0142)
    [    1.888311] nand: No NAND device found
    [    1.892082] omap2-nand 8000000.nand: scan failed, may be bus-width mismatch
    [    1.901214] m25p80 spi32766.0: found n25q00, expected s25fl256s1
    [    1.907338] m25p80 spi32766.0: n25q00 (131072 Kbytes)
    [    1.912468] 7 ofpart partitions found on MTD device spi32766.0
    [    1.918347] Creating 7 MTD partitions on "spi32766.0":
    [    1.923510] 0x000000000000-0x000000040000 : "QSPI.SPL"
    [    1.929640] 0x000000040000-0x000000140000 : "QSPI.u-boot"
    [    1.945957] 0x000000140000-0x0000001c0000 : "QSPI.u-boot-spl-os"
    [    1.952905] 0x0000001c0000-0x0000001d0000 : "QSPI.u-boot-env"
    [    1.969599] 0x0000001d0000-0x0000001e0000 : "QSPI.u-boot-env.backup1"
    [    1.986993] 0x0000001e0000-0x0000009e0000 : "QSPI.kernel"
    [    2.003367] 0x0000009e0000-0x000002000000 : "QSPI.file-system"
    [    2.016338]  nvme0n1: p1
    [    2.021187] libphy: Fixed MDIO Bus: probed
    [    2.076924] davinci_mdio 48485000.mdio: davinci mdio revision 1.6
    [    2.083050] libphy: 48485000.mdio: probed
    [    2.090202] davinci_mdio 48485000.mdio: phy[2]: device 48485000.mdio:02, driver TI DP83867
    [    2.099159] cpsw 48484000.ethernet: Detected MACID = 64:33:db:4b:8f:38
    [    2.105804] cpsw 48484000.ethernet: cpts: overflow check period 800
    [    2.112784] cpsw 48484000.ethernet: cpsw: Detected MACID = 64:33:db:4b:8f:39
    [    2.121409] mousedev: PS/2 mouse device common for all mice
    [    2.137610] i2c /dev entries driver
    [    2.146299] omap_hsmmc 4809c000.mmc: Got CD GPIO
    [    2.187642] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr25 mode
    [    2.194030] omap_hsmmc 480b4000.mmc: no pinctrl state for sdr12 mode
    [    2.217042] evm_3v3_sw: supplied by sysen1
    [    2.277731] ledtrig-cpu: registered to indicate activity on CPUs
    [    2.287823] aic_dvdd: supplied by evm_3v3_sw
    [    2.293064] davinci-mcasp 4847c000.mcasp: invalid tdm slots: 0
    [    2.300575] NET: Registered protocol family 10
    [    2.315878] sit: IPv6 over IPv4 tunneling driver
    [    2.321091] NET: Registered protocol family 17
    [    2.325768] Key type dns_resolver registered
    [    2.330214] omap_voltage_late_init: Voltage driver support not added
    [    2.337121] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
    [    2.343331] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
    [    2.350040] Adding alias for supply vdd,cpu0 -> vdd,4a003b20.oppdm
    [    2.356248] Adding alias for supply vbb,cpu0 -> vbb,4a003b20.oppdm
    [    2.363580] Power Management for TI OMAP4+ devices.
    [    2.368712] Registering SWP/SWPB emulation handler
    [    2.374840] dmm 4e000000.dmm: workaround for errata i878 in use
    [    2.382384] dmm 4e000000.dmm: initialized all PAT entries
    [    2.388823] [drm] Initialized omapdrm 1.0.0 20110917 on minor 1
    [    2.406677] hctosys: unable to open rtc device (rtc0)
    [    2.423717] evm_1v8: disabling
    [    2.426796] aic_dvdd: disabling
    [    2.430174] ldousb: disabling
    [    2.433660] ALSA device list:
    [    2.436640]   No soundcards found.
    [    2.440947] Waiting for root device PARTUUID=3cc717e1-02...
    [    2.467787] mmc0: host does not support reading read-only switch, assuming write-enable
    [    2.481494] mmc0: new high speed SDHC card at address aaaa
    [    2.487480] mmcblk0: mmc0:aaaa SL16G 14.8 GiB 
    [    2.496614]  mmcblk0: p1 p2
    [    2.550169] EXT4-fs (mmcblk0p2): couldn't mount as ext3 due to feature incompatibilities
    [    2.561302] EXT4-fs (mmcblk0p2): couldn't mount as ext2 due to feature incompatibilities
    [    2.714182] EXT4-fs (mmcblk0p2): recovery complete
    [    2.720290] EXT4-fs (mmcblk0p2): mounted filesystem with ordered data mode. Opts: (null)
    [    2.728465] VFS: Mounted root (ext4 filesystem) on device 179:2.
    [    2.740559] devtmpfs: mounted
    [    2.743751] Freeing unused kernel memory: 336K
    [    2.748236] This architecture does not have kernel memory protection.
    [    2.949343] systemd[1]: System time before build time, advancing clock.
    [    2.993692] random: systemd: uninitialized urandom read (16 bytes read, 17 bits of entropy available)
    [    3.009287] random: systemd: uninitialized urandom read (16 bytes read, 17 bits of entropy available)
    [    3.020981] systemd[1]: systemd 229 running in system mode. (+PAM -AUDIT -SELINUX +IMA -APPARMOR +SMACK +SYSVINIT +UTMP -LIBCRYPTSETUP -GCRYPT +GNUTLS +ACL +XZ -LZ4 -SECCOMP +BLKID -ELFUTILS +KMOD -IDN)
    [    3.039594] systemd[1]: Detected architecture arm.
    
    Welcome to Arago 2016.12!
    
    [    3.070721] systemd[1]: Set hostname to <dra7xx-evm>.
    [    3.146719] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 18 bits of entropy available)
    [    3.153906] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 18 bits of entropy available)
    [    3.154078] random: systemd-gpt-aut: uninitialized urandom read (16 bytes read, 18 bits of entropy available)
    [    3.201660] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 20 bits of entropy available)
    [    3.221869] random: systemd-sysv-ge: uninitialized urandom read (16 bytes read, 21 bits of entropy available)
    [    3.254125] random: systemd: uninitialized urandom read (16 bytes read, 22 bits of entropy available)
    [    3.263687] random: systemd: uninitialized urandom read (16 bytes read, 22 bits of entropy available)
    [    3.273667] random: systemd: uninitialized urandom read (16 bytes read, 22 bits of entropy available)
    [    3.563564] systemd[1]: Configuration file /etc/systemd/system/multi-user.target.wants/vsdk.service is marked executable. Please remove executable permission bits. Proceeding anyway.
    [    3.583544] systemd[1]: [/etc/systemd/system/multi-user.target.wants/vsdk.service:3] Failed to add dependency on rc.pvr, ignoring: Invalid argument
    [    3.699304] systemd[1]: sysinit.target: Found ordering cycle on sysinit.target/start
    [    3.707121] systemd[1]: sysinit.target: Found dependency on alignment.service/start
    [    3.714820] systemd[1]: sysinit.target: Found dependency on basic.target/start
    [    3.722117] systemd[1]: sysinit.target: Found dependency on sockets.target/start
    [    3.729573] systemd[1]: sysinit.target: Found dependency on dbus.socket/start
    [    3.736744] systemd[1]: sysinit.target: Found dependency on sysinit.target/start
    [    3.744272] systemd[1]: sysinit.target: Breaking ordering cycle by deleting job alignment.service/start
    [    3.753734] systemd[1]: alignment.service: Job alignment.service/start deleted to break ordering cycle starting with sysinit.target/start
    [ SKIP ] Ordering cycle found, skipping alignment.service
    [    3.789457] systemd[1]: Listening on udev Kernel Socket.
    [  OK  ] Listening on udev Kernel Socket.
    [    3.817359] systemd[1]: Started Dispatch Password Requests to Console Directory Watch.
    [  OK  ] Started Dispatch Password Requests to Console Directory Watch.
    [    3.847278] systemd[1]: Started Forward Password Requests to Wall Directory Watch.
    [  OK  ] Started Forward Password Requests to Wall Directory Watch.
    [    3.877212] systemd[1]: Listening on Syslog Socket.
    [  OK  ] Listening on Syslog Socket.
    [    3.897204] systemd[1]: Listening on /dev/initctl Compatibility Named Pipe.
    [  OK  ] Listening on /dev/initctl Compatibility Named Pipe.
    [    3.927111] systemd[1]: Reached target Swap.
    [  OK  ] Reached target Swap.
    [    3.960351] systemd[1]: Listening on Journal Socket.
    [  OK  ] Listening on Journal Socket.
    [    3.987382] systemd[1]: Listening on Network Service Netlink Socket.
    [  OK  ] Listening on Network Service Netlink Socket.
    [    4.017122] systemd[1]: Reached target Remote File Systems.
    [  OK  ] Reached target Remote File Systems.
    [    4.048570] systemd[1]: Created slice User and Session Slice.
    [  OK  ] Created slice User and Session Slice.
    [    4.077201] systemd[1]: Listening on Journal Socket (/dev/log).
    [  OK  ] Listening on Journal Socket (/dev/log).
    [    4.107203] systemd[1]: Listening on udev Control Socket.
    [  OK  ] Listening on udev Control Socket.
    [    4.138020] systemd[1]: Reached target Paths.
    [  OK  ] Reached target Paths.
    [    4.157743] systemd[1]: Created slice System Slice.
    [  OK  ] Created slice System Slice.
    [    4.227328] systemd[1]: Starting Journal Service...
             Starting Journal Service...
    [    4.257972] systemd[1]: Created slice system-getty.slice.
    [  OK  ] Created slice system-getty.slice.
    [    4.287980] systemd[1]: Created slice system-serial\x2dgetty.slice.
    [  OK  ] Created slice system-serial\x2dgetty.slice.
    [    4.357170] systemd[1]: Mounting Debug File System...
             Mounting Debug File System...
    [    4.389526] systemd[1]: Starting Setup Virtual Console...
             Starting Setup Virtual Console...
    [    4.419837] systemd[1]: Starting Create list of required static device nodes for the current kernel...
             Starting Create list of required st... nodes for the current kernel...
    [    4.464318] systemd[1]: Starting Load Kernel Modules...
             Starting Load Kernel Modules...
    [    4.480362] systemd[1]: Mounting POSIX Message Queue File System...
             Mounting POSIX Message Queue File System...
    [    4.519824] systemd[1]: Starting Remount Root and Kernel File Systems...
             Starting Remount Root and Kernel File Systems...
    [    4.539525] EXT4-fs (mmcblk0p2): re-mounted. Opts: (null)
    [    4.553170] systemd[1]: Mounting Temporary Directory...
             Mounting Temporary Directory...
    [    4.577868] systemd[1]: Reached target Slices.
    [  OK  ] Reached target Slices.
    [    4.604498] systemd[1]: Mounted Debug File System.
    [  OK  ] Mounted Debug File System.
    [    4.627281] systemd[1]: Mounted POSIX Message Queue File System.
    [  OK  ] Mounted POSIX Message Queue File System.
    [    4.657187] systemd[1]: Mounted Temporary Directory.
    [  OK  ] Mounted Temporary Directory.
    [    4.687408] systemd[1]: Started Journal Service.
    [  OK  ] Started Journal Service.
    [  OK  ] Started Setup Virtual Console.
    [  OK  ] Started Create list of required sta...ce nodes for the current kernel.
    [FAILED] Failed to start Load Kernel Modules.
    See 'systemctl status systemd-modules-load.service' for details.
    [  OK  ] Started Remount Root and Kernel File Systems.
             Starting udev Coldplug all Devices...
             Starting Apply Kernel Variables...
             Starting Create Static Device Nodes in /dev...
             Starting Flush Journal to Persistent Storage...
    [  OK  ] Started Apply Kernel Variables.
    [  OK  ] Started Create Static Device Nodes in /dev.
    [    5.450775] systemd-journald[106]: Received request to flush runtime journal from PID 1
    [  OK  ] Reached target Local File Systems (Pre).
             Mounting /media/ram...
             Mounting /var/volatile...
             Starting udev Kernel Device Manager...
    [  OK  ] Mounted /var/volatile.
    [  OK  ] Mounted /media/ram.
    [  OK  ] Started Flush Journal to Persistent Storage.
    [  OK  ] Started udev Kernel Device Manager.
    [    5.926601] omap-rproc 55020000.ipu: assigned reserved memory node ipu2_cma@95800000
    [    5.960330]  remoteproc0: 55020000.ipu is available
    [    5.970026]  remoteproc0: Note: remoteproc is still under development and considered experimental.
    [    6.009931]  remoteproc0: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
    [  OK  ] Reached target Local File Systems.
    [    6.052180] omap-rproc 40800000.dsp: assigned reserved memory node dsp1_cma@99000000
    [    6.061361]  remoteproc1: 40800000.dsp is available
    [    6.068848]  remoteproc1: Note: remoteproc is still under development and considered experimental.
             Starting Create Volatile Files and Directories...
    [    6.112439]  remoteproc1: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
             Starting Load/Save Random Seed...
    [    6.154468]  remoteproc1: Direct firmware load for dra7-dsp1-fw.xe66 failed with error -2
    [    6.172700] omap-rproc 41000000.dsp: assigned reserved memory node dsp2_cma@9f000000
    [    6.186199]  remoteproc1: failed to load dra7-dsp1-fw.xe66
    [  OK  ] Started udev Coldplug all Devices.[    6.209871]  remoteproc2: 41000000.dsp is available
    
    [    6.251763]  remoteproc2: Note: remoteproc is still under development and considered experimental.
    [    6.293628]  remoteproc2: THE BINARY FORMAT IS NOT YET FINALIZED, and backward compatibility isn't yet guaranteed.
    [  OK  ] Started Load/Save Random Seed.
    [    6.354977]  remoteproc2: Direct firmware load for dra7-dsp2-fw.xe66 failed with error -2
    [    6.370943]  remoteproc2: failed to load dra7-dsp2-fw.xe66
    [    6.401544]  remoteproc0: registered virtio0 (type 7)
    [  OK  ] Started Create Volatile Files and Directories.
    [    6.424814] omap_rng 48090000.rng: OMAP Random Number Generator ver. 20
    [  OK  ] Found device /dev/ttyS0.
    [    6.461756] omap-des 480a5000.des: OMAP DES hw accel rev: 2.2
    [    6.552187] omap_rtc 48838000.rtc: rtc core: registered 48838000.rtc as rtc0
             Starting Update UTMP about System Boot/Shutdown...
             Starting Network Time Synchronization...
    [    6.934338] omap-sham 4b101000.sham: hw accel on OMAP rev 4.3
    [    6.978565] CAN device driver interface
    [    7.013724] SCSI subsystem initialized
    [  OK  ] Started Network Time Synchronization.
    [    7.055790] omap-aes 4b500000.aes: OMAP AES hw accel rev: 3.3
    [  OK  ] Started Update UTMP about System Boot/Shutdown.
    [    7.103353] omap-aes 4b700000.aes: OMAP AES hw accel rev: 3.3
    [    7.116400] c_can_platform 4ae3c000.can: c_can_platform device registered (regs=fce3c000, irq=254)
    [  OK  ] Reached target System Time Synchronized.
    [    7.379404] ahci 4a140000.sata: SSS flag set, parallel bus scan disabled
    [   7.396805] ahci 4a140000.sata: Enable 32-bit DMA instead of 64-bit.
             Starting Synchronize System and HW clocks...
    [    7.424354] ahci 4a140000.sata: AHCI 0001.0300 32 slots 1 ports 3 Gbps 0x1 impl platform mode
    [    7.478139] ahci 4a140000.sata: flags: 64bit ncq sntf stag pm led clo only pmp pio slum part ccc apst 
    [  OK  ] Started Synchronize System and HW clocks.
    [    7.547703] FAT-fs (mmcblk0p1): Volume was not properly unmounted. Some data may be corrupt. Please run fsck.
    [    7.554494] scsi host0: ahci
    [    7.554864] ata1: SATA max UDMA/133 mmio [mem 0x4a140000-0x4a1410ff] port 0x100 irq 240
    [    7.576522] [drm] Initialized pvr 1.14.3699939 20110701 on minor 2
    [    7.906954] ata1: SATA link down (SStatus 0 SControl 300)
    [  OK  ] Listening on Load/Save RF Kill Switch Status /dev/rfkill Watch.
    [    7.933194] EXT4-fs (nvme0n1p1): recovery complete
    [  OK  ] Reached target System Initialization.
    [  OK  ] Started Daily Cleanup of Temporary Directories.[    7.953627] EXT4-fs (nvme0n1p1): mounted filesystem with ordered data mode. Opts: (null)
    
    [  OK  ] Reached target Timers.
    [  OK  ] Listening on dropbear.socket.
    [  OK  ] Listening on D-Bus System Message Bus Socket.
    [  OK  ] Reached target Sockets.
    [  OK  ] Reached target Basic System.
    [  OK  ] Started D-Bus System Message Bus.
             Starting Network Service...
    [    8.333246]  remoteproc0: powering up 55020000.ipu
    [  OK  ] Started System Logging Service.
    [    8.359292]  remoteproc0: Booting fw image dra7-ipu2-fw.xem4, size 4396172
    [    8.366329] omap-iommu 55082000.mmu: 55082000.mmu: version 2.1
             Starting rc.pvr.service...
    [    8.405081] net eth0: initializing cpsw version 1.15 (0)
    [    8.418519] net eth0: initialized cpsw ale version 1.4
    [    8.423702] net eth0: ALE Table size 1024
    [    8.424690]  remoteproc0: remote processor 55020000.ipu is now up
    [   8.434232] virtio_rpmsg_bus virtio0: rpmsg host is online
             Starting Permit User Sessions...
    [  OK  ] Started Kernel Logging Service.
    [    8.467884] net eth0: phy found : id is : 0x2000a231
             Starting Login Service...
    [    8.476661] virtio_rpmsg_bus virtio0: creating channel rpmsg-proto addr 0x50
    [  OK  ] Started Launching Vision SDK App.[    8.509299] IPv6: ADDRCONF(NETDEV_UP): eth0: link is not ready
    
    [  OK  ] Started Permit User Sessions.
    [    8.545875] NET: Registered protocol family 41
    [    8.577001] PVR_K: UM DDK-(3699939) and KM DDK-(3699939) match. [ OK ]
    [  OK  ] Started Network Service.
    [  OK  ] Started rc.pvr.service.
             Starting weston.service...
             Starting Network Service...
    [  OK  ] Started Serial Getty on ttyS0.
    [  OK  ] Started Getty on tty1.
    [  OK  ] Started weston.service.
    [  OK  ] Started Network Service.
    [  OK  ] Started Login Service.
             Starting Network Service...
             Starting telnetd.service...
             Starting tiipclad-daemon.service...
    [  OK  ] Started Network Service.
    [  OK  ] Started telnetd.service.
    [  OK  ] Started tiipclad-daemon.service.
             Starting Network Service...
    [  OK  ] Started Network Service.
             Starting Network Service...
    [  OK  ] Started Network Service.
    [FAILED] Failed to listen on Network Service Bus Name.
    See 'systemctl status org.freedesktop.network1.busname' for details.
    [FAILED] Failed to start Network Service.
    See 'systemctl status systemd-networkd.service' for details.
    [  OK  ] Reached target Network.
             Starting Network Name Resolution...
    [  OK  ] Started Network Name Resolution.
    [   13.474492] cpsw 48484000.ethernet eth0: Link is Up - 1Gbps/Full - flow control rx/tx
    [   13.482418] IPv6: ADDRCONF(NETDEV_CHANGE): eth0: link becomes ready
    [   13.776771] EXT4-fs (nvme0n1p1): mounted filesystem with ordered data mode. Opts: (null)
    
     _____                    _____           _         _   
    |  _  |___ ___ ___ ___   |  _  |___ ___  |_|___ ___| |_ 
    |     |  _| .'| . | . |  |   __|  _| . | | | -_|  _|  _|
    |__|__|_| |__,|_  |___|  |__|  |_| |___|_| |___|___|_|  
                  |___|                    |___|            
    
    Arago Project http://arago-project.org dra7xx-evm ttyS0
    
    Arago 2016.12 dra7xx-evm ttyS0
    
    dra7xx-evm login: [   15.815250] DMA: Module install successful, device major num = 241 
    [   15.821964] DRV: Module install successful
    [   16.100081] omap_l3_noc 44000000.ocp: L3 application error: target 3 mod:2 (unclearable)
    [   16.108242] omap_l3_noc 44000000.ocp: L3 debug error: target 3 mod:2 (unclearable)
    

  • EVM 上的TDA2的具体型号有吗?参考板上使用的是 TDA2SXBTQABCQ1

  • U62这个选择开关以及相关电路保留。

    你能测量一下TDA2复位信号拉高时候U26的S0、S1,S2的输入电压么?

    仿真器有么?可以看寄存器么?

    EVM 上的TDA2的具体型号有吗?

    请参考MMWCAS-DSP-EVM设计文件里的信息。

    你是否有对比过TI EVM和你自己的板子上启动时候SDCLK 信号频率一致吗?

  • 从DEMO板的log信息,可以看到:DRAM: 4 GiB   而自己做的参考板只有2GB    这个不同点是否会导致BOOT起来后系统进入死循环。DEMO板去到 EMIF1上的DDR也会起不来。

    1.TDA2复位信号拉高时候U26的S0、S1,S2的输入电压  3.27V  0  0                 没有仿真器

    2.TI EVM和自己的板子上启动时候SDCLK 信号频率一致在400kHz左右。

  • Jack,

    请你修改一下TDA2 MLO文件里DDR的相关配置,配置为1个EMIF接口。

    我看你提供的log是linux的,应该是和mmwave studio配套的sd卡image,相关源码请从下面的网址下载:

    PROCESSOR-SDK-VISION_03.07.01.00 | TI.com

    如果后续你有关于如何修改MLO以及相关编译问题,请到处理器相关论坛询问。