目前公司准备采购6843AOP芯片自己制作外围电路,查看6843AOP芯片手册(图2)及6843AOPEVM的方框图(图1),发现芯片内部是没有集成FLASH的,而是通过QSPI外接了
MX25R1635。因为考虑自己制板,有以下几个问题想确认:
(1)6843AOP芯片内部是否集成有FLASH,导致必须使用QSPI外接FLASH芯片来存储烧录的程序?
(2)外接FLASH芯片选型的问题,是否只能采用和EVM板相同的FLASH-MX25R1635,是否有适配6843AOP芯片的FLASH清单?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.


目前公司准备采购6843AOP芯片自己制作外围电路,查看6843AOP芯片手册(图2)及6843AOPEVM的方框图(图1),发现芯片内部是没有集成FLASH的,而是通过QSPI外接了
MX25R1635。因为考虑自己制板,有以下几个问题想确认:
(1)6843AOP芯片内部是否集成有FLASH,导致必须使用QSPI外接FLASH芯片来存储烧录的程序?
(2)外接FLASH芯片选型的问题,是否只能采用和EVM板相同的FLASH-MX25R1635,是否有适配6843AOP芯片的FLASH清单?
1. 芯片内部没有集成flash,需要使用外接flash。
2. 不需要和EVM相同,可以根据下面文档的要求选择合适的flash。
IWR6x43 Flash Variants Supported by the mmWave Sensor (Rev. x)