This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: 4芯片级联射频板子 电源芯片替换问题

Part Number: AWR2243
Other Parts Discussed in Thread: LP87524P-Q1, LP87564-Q1,

TI的工作人员:

    您好。关于LP87564-Q1与LP87524P-Q1芯片替换存在一些问题:

    我在应用AWR2243雷达4芯片级联EVM板子的时候,AWR2243雷达4芯片级联EVM板的射频电源用的芯片是LP87524P-Q1,并输出1.8V,1V等电压。

   现在我想用LP87564-Q1去替换,我对比了两个芯片手册,芯片管脚是一样的,并且4相位典型电路也一样,并且在应用中都是关闭了外部时钟。

但是奇怪的是,我用LP87564-Q1直接替换掉雷达板子上的LP87524P-Q1, 电源输出电压是0V. 为什么电源芯片无法正常工作?