This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1843: iwr1843

Part Number: IWR1843


使用mmwave studio捕获数据,配置没用任何错误,但是无法收到数据,画图的时候会提示数据为0,板子上面的灯也没有闪烁,请问这么解决,

  • 请问测试的是哪个例程?

    mmwave studio的输出信息贴出来看一下。

  • 你好,输出语句如下

    [15:00:39] DLL Version : 1.0
    [15:00:39] [RadarAPI]: ar1.SelectCaptureDevice("DCA1000")
    [15:00:39] [RadarAPI]: Status: Passed
    [15:00:41] [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "12:34:56:78:90:12", 4096, 4098)
    [15:00:41] [RadarAPI]: ar1.CaptureCardConfig_Mode(1, 2, 1, 2, 3, 30)
    [15:00:41] [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25)
    [15:00:56] [RadarAPI]: ar1.GetCaptureCardDllVersion()
    [15:00:56] [RadarAPI]: Sending dll_version command to DCA1000
    [15:00:56] [RadarAPI]:
    [15:00:56] DLL Version : 1.0
    [15:00:56] [RadarAPI]: ar1.SelectCaptureDevice("DCA1000")
    [15:00:56] [RadarAPI]: Status: Passed
    [15:01:00] [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "12:34:56:78:90:12", 4096, 4098)
    [15:01:00] [RadarAPI]: ar1.CaptureCardConfig_Mode(1, 2, 1, 2, 3, 30)
    [15:01:00] [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25)
    [15:01:08] [RadarAPI]: ar1.CaptureCardConfig_EthInit("192.168.33.30", "192.168.33.180", "12:34:56:78:90:12", 4096, 4098)
    [15:01:08] [RadarAPI]: ar1.CaptureCardConfig_Mode(1, 2, 1, 2, 3, 30)
    [15:01:08] [RadarAPI]: ar1.CaptureCardConfig_PacketDelay(25)
    [15:01:16] [RadarAPI]: ar1.GetCaptureCardDllVersion()
    [15:01:17] [RadarAPI]: Sending dll_version command to DCA1000
    [15:01:17] [RadarAPI]:
    [15:01:17] DLL Version : 1.0
    [15:01:17] [RadarAPI]: ar1.SelectCaptureDevice("DCA1000")
    [15:01:17] [RadarAPI]: Status: Passed
    [15:01:20] [RadarAPI]: ar1.CaptureCardConfig_StartRecord("D:\\TI\\mmwave_studio_02_01_01_00\\mmWaveStudio\\PostProc\\adc_data.bin", 1)
    [15:01:25] [RadarAPI]: ar1.StartFrame()
    [15:01:25] [RadarAPI]: Status: Passed
    [15:01:25] Frame start async event received!
    [15:01:25] [RadarAPI]: Frame Ended
    [15:01:25] Frame End async event received!
    [15:01:28] [RadarAPI]: ar1.StartMatlabPostProc("D:\\TI\\mmwave_studio_02_01_01_00\\mmWaveStudio\\PostProc\\adc_data.bin")
    [15:01:28] [RadarAPI]: No of files Captured: 0, Total no of frames for each device : 8
    [15:01:28] Error : The number of files captured is zero!

  • Error : The number of files captured is zero!

    针对该报错,参考DCA1000 Debugging Handbook 看一下。

    1588.DCA1000 Debugging Handbook (1).pdf

    以下帖子中的讨论也看一下。

    e2echina.ti.com/.../672028