This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642: 1642程序堵塞

Part Number: AWR1642
Other Parts Discussed in Thread: SYSBIOS

你好,我在AWR1642EVM上跑基于SRR修改的程序,出现以下问题,请问有可能是什么问题?

[Cortex_R4_0] Debug: Launched the Initialization Task
[C674X_0] Heap L1 : size 16384 (0x4000), free 1216 (0x4c0)
Heap L3 : size 786432 (0xc0000), free 229376 (0x38000)
Heap L2 : size 49152 (0xc000), free 20464 (0x4ff0)
[Cortex_R4_0] Debug: Initialized the mmWave module
Debug: Synchronized the mmWave module
Debug: CLI is operational
Debug: MMWave has been configured for SRR.
Debug: Sensor will start momentarily.
Exception occurred in ThreadType_Task.
Task handle: 0x8000ea8.
Task stack base: 0x8000ef8.
Task stack size: 0x4000.
R0 = 0x2c50a524 R8 = 0x00000118
R1 = 0x2c50a524 R9 = 0x00000000
R2 = 0xffffff09 R10 = 0x52080004
R3 = 0x0800a924 R11 = 0x52080000
R4 = 0x0800a210 R12 = 0x0000001f
R5 = 0x5208011c SP(R13) = 0x08004e00
R6 = 0x0800a524 LR(R14) = 0x0800a904
R7 = 0x0000001c PC(R15) = 0x00007bde
PSR = 0x000c019f
DFSR = 0x0000000d IFSR = 0x00000000
DFAR = 0x2c50a524 IFAR = 0x00000000
ti.sysbios.family.arm.exc.Exception: line 205: E_dataAbort: pc = 0x00007bde, lr = 0x0800a904.
xdc.runtime.Error.raise: terminating execution