This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1843: 生成bin文件失败

Part Number: IWR1843


build 过程中出现以下问题

**** Build of configuration Debug for project vitalSigns_16xx_dss ****

"D:\\CCSV10\\CCSV10INSTALL\\ccs\\utils\\bin\\gmake" -k -j 8 all -O

rm -f D:/CCSV10/CCS_V10_WORKPLACE/vitalSigns_16xx_dss/vitalSigns_16xx_dss.bin
makefile:189: recipe for target 'pre-build' failed
process_begin: CreateProcess(NULL, rm -f D:/CCSV10/CCS_V10_WORKPLACE/vitalSigns_16xx_dss/vitalSigns_16xx_dss.bin, ...) failed.
make (e=2): 系统找不到指定的文件。

gmake[1]: [pre-build] Error 2 (ignored)

gmake[2]: 'vitalSigns_16xx_dss.xe674' is up to date.

**** Build Finished ****

在post-build加入以下命令后在debug文件夹下也不能生成.bin文件

"${CCS_INSTALL_ROOT}/utils/tiobj2bin/tiobj2bin" "${BuildArtifactFileName}" "${BuildArtifactFileBaseName}.bin" "${CG_TOOL_ROOT}/bin/armofd" "${CG_TOOL_ROOT}/bin/armhex" "${CCS_INSTALL_ROOT}/utils/tiobj2bin/mkhex4bin"