This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1843BOOST: 使用DCA1000EVM进行数据捕获的问题

Part Number: IWR1843BOOST
Other Parts Discussed in Thread: IWR1843

老师您好,通过阅读Ti使用手册知道,我们收到的信号实际上是Tx信号和Rx信号通过混频器后,再通过一次低通滤波器后得到的中频信号(IF),在这里我有两个问题:

(1)IWR1843 BOOST是有4G的带宽(77~81GHz),我们收到的IF信号是否会丢失真实的4G带宽的一些信息呢?

(2)我们收到IF信号,能不能反推出Rx信号啊?因为我觉得Rx信号才可以真实的反应出4G的带宽信息,不知道我的理解是否正确。望老师解惑,谢谢!