This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2944EVM: AWR2944 high end corner radar角雷达demo 波形参数配置问题

Part Number: AWR2944EVM


如图所示相关配置中,有两个相关问题不清晰

问题1:

profileCfg 1 77 6.24 0 46.05 0 0 9.761 0 512 0 0 0 44 

命令行所示配置命令中,起始频率为77Ghz,此处参数为77

但是code注释中LSB为53.664Hz,如何实现通过LSB配置参数与77Ghz的转换(转换关系)?

问题2:

实现雷达chirp跳频配置时,chirp相关参数有startFreqVar与freqSlopeVar

此处startFreqVar是否为chirp跳频的总频率?