This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: 使用dca1000evm和iwr1642boost进行数据采集报错“Ethernet Cable is disconnected Please check.....!!!”

Part Number: DCA1000EVM


我的设备是dca1000evm+iwr642boost,在使用mmwave studio进行数据采集时,点击Set Up DCA1000的connect时,报错“ConnectRFDCCard Status: RFDCCARD_UDP_WRITE_ERR
Ethernet Cable is disconnected Please check.....!!!”

我已经反复确认了防火墙已经关闭,并且设置好了静态ip地址,更换了多条网线。该问题依然存在。

我的mmwave studio 版本是2.0.0.2

请问这种情况如何解决?

谢谢