This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843AOP: 电源电压LDO bypass相关

Part Number: IWR6843AOP


TI工程师您好

有个LDO bypass 的问题想请教下:

 

背景:IWR6843AOP模块 ,firmware use 3D_people_count_demo.bin

问题1:其中在3D_people_count_mss工程mss_main.c文件下有关于.ldoBypassEnable参数默认为0,我从代码里的注释里发现了相矛盾的地方,想知道该配置是bypass启用了还是没启用?另外有相关的文档可以提供下吗?

.

问题2:我在IWR6843AOP Single-Chip 60- to 64-GHz mmWave Sensor Antennas-On-Package (002).pdf手册中看到有关发送器数目的说明:

目前有三路发送器,假设编号①、②、③

1、 外部提供1.0V电源输入,内部LDO 旁路:可同时启用3路发送器,有七种情况:①、②、③、①②、①③、②③、①②③

2、 外部提供1.3V电源输入,内部LDO启用:仅能启用两路发送器,有六种情况:①、②、③、①②、①③、②③

想确认下 按我的理解上面列举出的七种情况和六种情况我列举的对吗?这些种情况都是可以正常工作的吗?