AWR2243级联板+TDA2XX采集卡,需要什么供电标准
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
但是,《采用级联毫米波传感器的成像雷达参考设计》文档中提到,
The Cascade RF board accepts 5V DC, 8 A (max) power through the host board connectors. The primary
5 V system rail can be converted into the various AWR2243 device rails by a pair of LP87524P, quad
channel, monolithic, buck-converters
以哪个为准呢。目前我们用5V的电源,雷达也能正常工作。
另外,想问一下有没有推荐的电源,我们这边想买一个。
上面文档中提到的5v是级联板的电源要求。这个5V是由TDA2XX采集卡转换提供的。所以只需要给TDA2XX采集卡提供12v 5A的电源即可。可以看一下级联板的文档说明。
2.2 Attaching the MMWAVCAS-RF-EVM to the MMWAVCAS-DSP-EV
https://www.ti.com/cn/lit/ug/swru553a/swru553a.pdf
只要能提供12v 5A电源适配器都可以,TDA2采集板文档中列出的是advantech的适配器型号。
The typical power source is 12-V, 5-A Advantech Power supply P/N: 96PSA-A60W12V1-1.
https://www.ti.com/lit/ug/spruis6/spruis6.pdf