1、关于IWR6843AOP,有个WARMRST引脚,在EVM里面是上拉,这个引脚是什么作用,是IWR6843AOP的信号输出,还是输入?如果我这个引脚悬空的话,会出现什么问题?
2、我把SOP【2:0】设置成烧录模式时,重新上电,用uniflash烧录,发现flash的cs引脚都是高电平,没有被拉低,烧录失败:

寻求帮助
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1、关于IWR6843AOP,有个WARMRST引脚,在EVM里面是上拉,这个引脚是什么作用,是IWR6843AOP的信号输出,还是输入?如果我这个引脚悬空的话,会出现什么问题?
2、我把SOP【2:0】设置成烧录模式时,重新上电,用uniflash烧录,发现flash的cs引脚都是高电平,没有被拉低,烧录失败:

寻求帮助
1、用于软复位。输入输出都可以。

请参考hardware checklist对该引脚的描述:
WARM_RESET - special signal can be input or output, normally a pullup 3.3v output, 0->1 indicates SOC hardware init complete, or internal reset error
2、请问是第一次烧录程序吗?参考:
我确认一下再给你回复
WARM_RESET是开漏引脚,需要弱上拉到3.3v。请按照官方的建议来进行设计。
我是买芯片焊在自己的板子(板子是保留evm的mission部分)上,
保留mission部分什么意思?
在确保所有的操作步骤无误的情况下,如果是自制板,也可能是硬件问题导致的,手上有开发板吗?对比看一下。
HW bringup guideline: