1.在不同场景采集数据,是否需要在每个场景都采集一组校准矩阵。
2.对天线校准时,使用12发16收。而实际应用时使用6发16收,请问是否可以直接使用12发16收的校准矩阵,是否需要重新对天线进行校准。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,
校准建议在微波暗室里做一次。
如果是MIMO校准,是基于第一根发射天线和第一根接收天线的。使用6发16收,可以使用12发16收的校准数据。
The FFT index of TX1/RX1 channel is used as reference that is compared with all the other 191 channels.
建议你仔细阅读一下下面的文档,了解校准的原理。
mmwave_studio_03_00_00_14\mmWaveStudio\MatlabExamples\signal_processing_4chip_cascade.pdf