最近我在考虑去室外空旷的地方测一些数据,但是我发现三脚架很难固定雷达的板卡,角反倒是很好固定。

请问您这边一般是用什么固定的。谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
一般是用三脚架+手机夹固定,类似下面链接里这种。
The EVM needs to be mounted at a height of ~2.0-2.5m with a slight downtilt. An adjustable clamp style smartphone adapter mount for tripods and a 60-75" tripod can be used to clamp and elevate the EVM. This is only an example solution for mounting; other methods can be used so far as setup specifications are met.
https://dev.ti.com/tirex/explore/node?node=AKx-QpHUGv1KSGqjtILLQw__VLyFKFf__LATEST&r=AocYeEd__2.6.0&r=VLyFKFf__3.2.0&r=VLyFKFf__3.6.2&r=VLyFKFf__4.10.0