This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

MMWCAS-RF-EVM: 角度估计

Part Number: MMWCAS-RF-EVM


TI的工程师,你们好

  我最近在使用mmwcas-rf-evm这块板子做角度估计,遇到了一些问题:

1、之前询问过了有关内容,在使用虚拟天线做fft的时候有一步对速度校正来消除相位的影响

但是文档里面没有说具体怎么做,想问一下做这一步的目的是什么?是为了消除TDM模式下相邻chirp距离的变化而导致的相位变化吗?

2、在TDM模式下,使用MIMO的参数配置,接收矩阵维度为[samples,chirps,Rx,Tx],如果我仅选择一根Tx做angle fft,即选用的数据为data=[detected_s,detected_c,13:16,12],其中detected_s和detected_c为确定的常数,选用的接收天线序号为13、14、15、16,发送天线序号为12,matlab程序如下

angle_data = fftshift(fft(data,180));

[~,page] = max(abs(angle_data));

theta_azi(i,j) = asin((page-90-1)/180*lamda/(lamda/2))*180/pi;

为什么计算出来的theta_azi全部都是0°?

期待你们的回复。