This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: MMWAVCAS-RF-EVM级联板MSS Power Up async event was not received! Device 3 : SPI Connection Failed

Part Number: AWR2243

尊敬的TI工程师和论坛的朋友们:

我们在配置MMWAVCAS-RF-EVM级联板过程中,遇到了SPI connect(3)无法通过的问题。具体地说,我们运行了Cascade_Configuration_MIMO.lua来自动配置,device1 和device2 均能顺利完成配置,当进行到device3时出现下面的报错:

Fullscreen
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
[10:12:47] Setting up Studio for Cascade started..
[10:12:47] [RadarAPI]: Connection to the TDA is already established!
[10:12:47] ConnectTDA Successful
[10:12:47] selectCascadeMode Successful
[10:12:47] Setting up Studio for Cascade ended..
[10:12:47] [RadarAPI]: ar1.RemoveDevice(2)
[10:12:47] [RadarAPI]: Status: Passed
[10:12:47] [RadarAPI]: ar1.PowerOff_mult()
[10:12:47] [RadarAPI]: Status: Passed
[10:12:48] [RadarAPI]: Device 1 : CAPTURE_RESPONSE_ACK Async event recieved() with status 0
[10:12:48] [RadarAPI]: Device 1 : CAPTURE_RESPONSE_ACK Async event recieved() with status 0
[10:12:48] [RadarAPI]: ar1.FullReset(1)
[10:12:48] [RadarAPI]: Status: Passed
[10:12:48] [RadarAPI]: ar1.SOPControl_mult(1,4)
[10:12:48] [RadarAPI]: Status: Passed
[10:12:48] Master : SOP Reset Successful
[10:12:49] [DeviceId-0] MSS power up done async event received!
[10:12:49] [RadarAPI]: ar1.PowerOn_mult(1, 0, 1000, 0,0)
[10:12:49] [RadarAPI]: Status: Passed
[10:12:49] Master : SPI Connection Successful
[10:12:49] [RadarAPI]: ar1.DownloadBssFwOvSPI_mult(1, C:\\ti\\mmwave_dfp_02_02_03_01\\firmware\\xwr22xx_metaImage.bin)
XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX

尝试过手动配置,也出现了同样的错误。查阅了网络上各种论坛的资料,没能找到合适的解决方法,因此来求助各位,十分感谢!