Other Parts Discussed in Thread: UCC27531, TDC1000
我在看这个测试板的时候,对于这个电路有点疑惑,能看的懂这个电路的作用,但是不了解UCC27531这个芯片的用途是什么?他的普遍作用是干什么的?以及可以采用哪些其他芯片进行代替?

谢谢,您的观看,如果你了解这个,期待你的回复。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我在看这个测试板的时候,对于这个电路有点疑惑,能看的懂这个电路的作用,但是不了解UCC27531这个芯片的用途是什么?他的普遍作用是干什么的?以及可以采用哪些其他芯片进行代替?

谢谢,您的观看,如果你了解这个,期待你的回复。
您好,
您在哪里看到的这个电路?我在TDC1000-C2000EVM Design File的原理图中没找到这个电路
Hi
UCC27531是电源驱动器, 在一些驱动能力较小的芯片(Gate输出,例如峰值驱动电流仅仅1A,甚至更小)可以将驱动输出给到UCC27531进行驱动能力放大(此时驱动峰值电流就是UCC27531的,具体可以看其datasheet)