This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR1443: framecfg

Part Number: IWR1443


经测试,每个frame的时间为36毫秒

frameCfg 1 2 64 1 100 1 0 我如果这么设置参数,frame循环100多次之后就直接重启(测试过是重启)

如果  frameCfg 1 2 64 1 120 1 0  则系统能够一直自动的运行下去。

After testing, the time of each frame is 36ms.

frameCfg 1 2 64 1 100 1 0   If I set the parameters like this, the frame will restart directly after more than 100 cycles 

If frameCfg 1 2 64 1 120 1 0,   the system can always run automatically.

  • 请问只修改了framecfg的frame periodicity,还有修改其他参数么?frame periodicity是用来控制发帧的间隔的。增大间隔对射频部分来说应该是没有问题的。修改的是哪个demo?能连上仿真器看看在ccs console里是否有报什么错误?