Other Parts Discussed in Thread: TPSM831D31
我正考虑多片AWR2243级联的方案(几十片),是否可以使用一个大电流的DCDC为多颗awr2243提供电源?例如使用TPSM831D31输出1.0v和1.2v,并在改dcdc的输出只加一个总的LC滤波,在每个awr2243入口处仅做电容滤波,不额外增加滤波,这样是否可行?会有其他风险吗,例如不同awr2243之间的串扰风险吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我正考虑多片AWR2243级联的方案(几十片),是否可以使用一个大电流的DCDC为多颗awr2243提供电源?例如使用TPSM831D31输出1.0v和1.2v,并在改dcdc的输出只加一个总的LC滤波,在每个awr2243入口处仅做电容滤波,不额外增加滤波,这样是否可行?会有其他风险吗,例如不同awr2243之间的串扰风险吗?
你好,
AWR2243的电源要求请参考数据手册的8.5 Power Supply Specifications,其中有提到1.3V (1.0V) and 1.8V的电源的ripple是由特殊要求的,ripple太大会影响射频性能。还有就是选择的电源芯片的开关频率不能很低,不然会在中频信号里产生噪声。在AWR2243芯片电源输入前的滤波电路就是要滤除开关频率以及谐波。
建议还是使用TI推荐的PMIC的方案和电源电路设计。