This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1243BOOST: MCU 控制masted 1243,程序停止在 SensorStart部分

Part Number: AWR1243BOOST
Other Parts Discussed in Thread: AWR1243, AWR2243

硬件平台 : 4AWR1243 (AWRx Cascaded Radar RF Evaluation Module)+ARM MCU(GD32F3) ,

连接:SPI_CLK_1 SPI_CS_1 MOSI_1  MISO_1   SOP Control:  functional mode, 

           NRESET:信号线,SPI_IRQ线,CSI2线没有连接

mmwave-example-nonos可以再MCU运行,并且配置成功,但是程序卡在 SensorStart,收不到1243的应答。CSI 2线没有连接有影响吗

   mmwl_bSensorStarted = 0U;
    retVal = rlSensorStart(deviceMap);
#ifndef ENABLE_TEST_SOURCE
    if ((rfDevCfg.aeControl & 0x1) == 0x0)
    {
        while (mmwl_bSensorStarted == 0U)
        {
            osiSleep(1); /*Sleep 1 msec*/
            timeOutCnt++;
            if (timeOutCnt > MMWL_API_RF_INIT_TIMEOUT)
            {
                retVal = RL_RET_CODE_RESP_TIMEOUT;
                break;
            }
        }
    }