This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1843BOOST: 68和18

Part Number: AWR1843BOOST


您好,

我使用的demo为:D:\ZJ\mmwave_industrial_toolbox_4_11_0\labs\Level_Sensing

我的开发板是AWR1843BOOST,然后我需要做一个levelsensing的代码,我看到TI给出的代码只有16和68的,但是由于18和68高度相似,因此很多68的代码可以在18上运行,所以我把68的levelsense的代码写入1843,在输入配置文件之前,一切正常。由于68和18的chirp起始频率不一样,所以我将68的cfg中的起始频率改为77GHZ。然后我将其通过串口输入,但是最后返回以下错误代码

我的配置文件如下,我改动了profileCfg的第二个参数,从60改动为了77,这个是起始频率的值

flushCfg
dfeDataOutputMode 1
channelCfg 8 1 0
adcCfg 2 1
adcbufCfg 0 1 1 1
profileCfg 0 77 7 7 114.4 0 0 33.71 1 512 5000 0 0 48
chirpCfg 0 0 0 0 0 0 0 1
frameCfg 0 0 2 0 500 1 0
lowPower 0 0
guiMonitor 1 1 0 0 0 1
RangeLimitCfg 2 1 0.3 3.0
sensorStart

我自己查询error.h和mmwave.h认为错误出在:@brief Error Code: mmWave link BSS calibration configuration failed
*/
#define MMWAVE_ECALCFG (MMWAVE_ERRNO_BASE-19)

我的问题如下:

1.68的代码是否有一些是可以在18上运行的

2.我这个问题该如何解决,有无解决的方向