Other Parts Discussed in Thread: AWR1642
尊敬的工程师,您好!对于TI雷达硬件触发我有以下几个问题:
1.硬件触发的模式和mmwave studio的软件触发模式的区别是啥?比如我在mmwave studio设置了发10帧,一帧loops为1,帧间隔100ms。那么我使用脉冲触发是只用触发一次就可以了吗?如果只需要触发一次就启动,那么我采用无限发的模式,怎么停止呢?
2.AWR2243的级联板能否采用硬件触发?
期待得到您的回复!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
1. 硬件触发需要在sync_in引脚输入触发信号。如果你在framecfg里面设置no of frame为10并且使用hardware trigger。那当外部输入一个同步脉冲,芯片就会发送10个frame。
2. 可以看一下mmwave_studio_cascade_user_guide.pdf文档
For Frame Configuration, select the “Hardware Trigger” for all the enabled slave devices and “Software Trigger” for Master device.
1. 既然是无限发模式,就不会停。
2. AWR2243有sync_in引脚,请参考数据手册。
https://www.ti.com/lit/ds/symlink/awr2243.pdf
级联板中没有sync_in引出,slave的sync_in信号由master提供。可以参考一下下面的cascade文档说明。
https://www.ti.com/lit/an/swra574b/swra574b.pdf