This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FDC1004: 请问FDC1004作为液位检测时可以检测的距离

Part Number: FDC1004


各位专家好:

 目前我在设计一款液位检测的PCB 板,使用贵司的FDC1004芯片。我们需求的是我设计的PCB 板和待测液位之间距离3到5cm,在这个距离内可以检测到液位变化。简易图如下。

目前我们在这个距离无法检测到对应的电荷变化,如果距离为0cm(紧贴容器璧)可以测到电荷变化。

请问如何做到3到5cm的电荷变化?

谢谢: