Other Parts Discussed in Thread: UNIFLASH, IWR6843ISK,
1、使用MMWAVEICBBOOST板卡搭配iwr 6843ISK板卡调试,之前多次使用XDS110调试、连接、运行,操作都没有问题;
2、今天无意没有连接USB 线缆情况下进入调试,报错,后多次重启板卡、断电、电脑重启等,还是连接出现问题,出现以下报错,

IcePick_M_0: Error connecting to the target: (Error -2131 @ 0x0) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.4.0.00129)
CS_DAP_0: Error connecting to the target: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 9.4.0.00129)
3、单独烧写iwr 6843ISKflash可以,但是无法解决XDS110连接问题。
调试紧张,麻烦给出合适的解决办法