This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPT3101-SDK: 使用OPT3101-SDK的代码配置为去混叠模式模式,频率无法正常自动切换

Part Number: OPT3101-SDK


您好!

我们参考OPT3101-EVM设计的测距模块,使用了TI官网的OPT3101-SDK的代码,初始化模块为普通非HDR连续读模式。在这个模式下将系统分别单独配置为默认10MHz和去混叠8.57MHz时,校准和测量都是正常的。但是校准好串扰和相位偏差,同时初始化好8.57MHz时的ALPHA1_DEAL_SCAL、BETA1_DEAL_SCAL、PHASE2_OFFSET_HDR0_TX0、PHASE2_OFFSET_HDR1_TX0这几个寄存器,配置为去混叠模式后,系统不会自动正常切换频率,请问这可能是什么原因?此时,mod_freq打印值会在0和1之间交替变化,但是发射管几乎没有什么电流输出,用示波器测量发射管脉冲频率一直都是10MHz。

参考了TI论坛的一些帖子,但是仍未完全解决我的问题:

OPT3101: using dealias mode

OPT3101: How to perform dealiasing? If I want to measure a distance greater than 15 meters

相关调试信息如下:

1. 寄存器初始化代码

void OPT3101::device::initializeDealiasTest(void){
    // List of registers to initialize OPT3101 device after power-up

	this->reg.force_en_slave = 1; // //Since I2C Master bus is floating this register needs to be set to enable device to respond

	this->reg.tg_ovl_window_start = 7000; // //Overload flab observation window
	this->reg.en_temp_conv = 1; // //Enables the internal

	this->reg.clip_mode_fc = 0; // //Enables Clip mode for Frequency correction
	this->reg.clip_mode_temp = 0; // //Disables Clip mode for Temp coff phase correction
	this->reg.clip_mode_offset = 0; // //Disables Clip mode for phase offset correction
	this->reg.iq_read_data_sel = 3; // //Enables 16 bit frame counter
	this->reg.iamb_max_sel = 14; // 12=100uA, 14=200uA //Sets maximum ambient support
	this->reg.en_temp_corr = 1;
	this->reg.gpio1_obuf_en=1; // //Enabled output buffer on GPIO1 pin
	this->reg.gpo1_mux_sel=2; 	    // //select dig_gpo_0 on gpio1
	this->reg.dig_gpo_sel0 = 9; 	// //Select Data Ready on dig_gpo_0

	this->reg.num_sub_frames = 63; // //Sub frames count
	this->reg.num_avg_sub_frames = 63; // //Average frames count
	this->reg.xtalk_filt_time_const = 4; // //Crosstalk filter time constant
	this->reg.tg_seq_int_start 	= 9850; // //Sequence Start
	this->reg.tg_seq_int_end 		= 9858; // //Sequence End
	this->reg.tg_seq_int_mask_start 	= 63; // //Same as AvgFrame Count
	this->reg.tg_seq_int_mask_end 	= 63; // //Same as AvgFrame Count

    this->reg.illum_dac_h_tx0 = 18; // //High Current settings: [173.6mA:5.6mA X 31], [078.4mA:5.6mA X 14], [067.2mA:5.6mA X 12]
	this->reg.illum_scale_h_tx0 = 0; // //Illum scale for H: 0=5.6mA, 1=4.2mA

	this->reg.sel_hdr_mode = 1; // //Selecting H Channel by default

    this->reg.tx_seq_reg   = 2184; // //Setting TX Switching order
	this->reg.en_tx_switch = 0; // //Enable TX Switching order
    
    //this->reg.override_clkgen_reg = 1;                  // 将此寄存器设置为 1 可允许用户独立控制 DEALIAS_FREQ、 DEALIAS_EN。
    //this->reg.dealias_en = 1;                           // 更改调制频率,去混叠使能。 仅当 OVERRIDE_CLKGEN_REG = 1 时, 此寄存器才有效。
    //this->reg.en_multi_freq_phase = 1;                  // 如果此位设置为 1 且 EN_DEALIAS_MEAS = 1, 则 PHASE_OUT 寄存器为相位测量提供两个频率。 相位的频率在 MOD_FREQ 状态位中指示。0: 10MHz 调制 | 1: 10MHz 和 10 × (6 / 7) MHz 或 10 × (6 / 5) MHz 调制
    //this->reg.dealias_freq = 0;                         // 当 DEALIAS_EN = 1 时, 选择调制频率。 仅当 OVERRIDE_CLKGEN_REG = 1 时, 此寄存器才有效。0: 10 × (6 / 7) MHz | 1: 10 × (6 / 5) MHz。
    
    this->reg.command0 = 0x100; // Set to fo = 10MHz
    this->reg.command1 = 0x102; // Set to fo to de-alias frequency
    this->reg.command2 = 0x400; // Go to Command0
    
    this->reg.ncr_config = 0;                           // 选择第二个频率进行去混叠操作。0: 10 × (6 / 7) MHz |     1: 10 × (6 / 5) MHz。
    this->reg.give_dealias_data = 1;                    // 此寄存器设置为 1 时, 在 PHASE_OUT 上发出去混叠的相位。
    this->reg.en_sequencer = 1;                         // 启用序列发生器。0: 启用序列发生器 | 1: 禁用序列发生器。
    this->reg.en_processor_values = 1;                  // 使用STATUS_OUT值而不是寄存器值。
    //this->reg.en_dealias_meas = 1;                    // do it in command1 // 启用去混叠测量。0: 默认工作模式 | 1: 去混叠工作模式
    
	this->reg.tg_en = 1; // //Enables Timing Generator

	this->configurationFlags_xtalkFilterTau =  4; // //This is not a register but a settings flag for the SDK
	this->configurationFlags_monoshotMode =  false; // //This is not a register but a settings flag for the SDK
	this->configurationFlags_xtalkSettlingOneTauInMilliSeconds      =  256; // //This is not a register but a settings flag for the SDK
	this->configurationFlags_xtalkSettlingOneTauInDataReadyCounts   =  16; // //This is not a register but a settings flag for the SDK
	this->configurationFlags_frameTimeInMilliSeconds                =  16; // //This is not a register but a settings flag for the SDK
	this->configurationFlags_avgFrameCountExponentOfTwo             =  6; // //This is not a register but a settings flag for the SDK
}

OPT3101::device::device(void):
configurationFlags_isTXChannelActive{true,false,false},
configurationFlags_isRegisterSetActive{false,true} {}

OPT3101::calibrationC::calibrationC(void) : calibrationC(true) {
	this->recordLength           = 1; // //This configuration requires 1 crosstalk and other configuration record(s)
	this->registerAddressListSize= 17; // //This configuration requires 17 registers [544] bits to be stored for calibration
	this->EEPROM_connected       =  false; // //This configuration helps configure EEPROM
	this->extTempSensor_connected=  false; // //This configuration helps configure Ext temp sensor
	this->registerAddressList[0] = 0x31; // //Address for register(s) iphase_xtalk_reg_hdr1_tx0
	this->registerAddressList[1] = 0x32; // //Address for register(s) qphase_xtalk_reg_hdr1_tx0
	this->registerAddressList[2] = 0x5e; // //Address for register(s) temp_coeff_xtalk_iphase_hdr1_tx0
	this->registerAddressList[3] = 0x60; // //Address for register(s) temp_coeff_xtalk_qphase_hdr1_tx0
	this->registerAddressList[4] = 0x51; // //Address for register(s) phase_offset_hdr1_tx0,temp_coeff_illum_hdr1_tx0
	this->registerAddressList[5] = 0x48; // //Address for register(s) tmain_calib_hdr1_tx0,tillum_calib_hdr1_tx0
	this->registerAddressList[6] = 0x2d; // //Address for register(s) temp_coeff_main_hdr1_tx0
	this->registerAddressList[7] = 0x52; // //Address for register(s) temp_coeff_illum_hdr1_tx0
	this->registerAddressList[8] = 0x2e; // //Address for register(s) illum_xtalk_reg_scale
	this->registerAddressList[9] = 0x3a; // //Address for register(s) scale_temp_coeff_xtalk
	this->registerAddressList[10] = 0x71; // //Address for register(s) shift_illum_phase
	this->registerAddressList[11] = 0x43; // //Address for register(s) en_phase_corr,en_temp_corr,scale_phase_temp_coeff
	this->registerAddressList[12] = 0xb5; // //Address for register(s) scale_amb_phase_corr_coeff
	this->registerAddressList[13] = 0x0c; // //Address for register(s) amb_phase_corr_pwl_coeff0
	this->registerAddressList[14] = 0xb4; // //Address for register(s) amb_phase_corr_pwl_coeff1,amb_phase_corr_pwl_coeff2,amb_phase_corr_pwl_coeff3
	this->registerAddressList[15] = 0xb8; // //Address for register(s) amb_phase_corr_pwl_x0,amb_phase_corr_pwl_x1
	this->registerAddressList[16] = 0xb9; // //Address for register(s) amb_phase_corr_pwl_x2
}

非常感谢您的回复!