This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: 修改配置

Part Number: IWR6843ISK


您好,我使用的是

D:\zj\AutomotiveToolbox\mmwave_industrial_toolbox_4_1_0\labs\people_counting\68xx_people_counting

我想问一下,这个配置是否能够改为3个TX。我看到原始配置如下:

flushCfg
dfeDataOutputMode 1
channelCfg 15 5 0
adcCfg 2 1
adcbufCfg 0 1 1 1
profileCfg 0 60.6 30 10 62 0 0 53 1 128 2500 0 0 30
chirpCfg 0 0 0 0 0 0 0 1
chirpCfg 1 1 0 0 0 0 0 4
frameCfg 0 1 128 0 50 1 0
lowPower 0 1
guiMonitor 1 1 0 0
cfarCfg 6 4 4 4 4 16 16 4 4 55 67 0
doaCfg 600 1875 30 1 1 0
SceneryParam -6 6 0.5 6
GatingParam 3 2 2 0
StateParam 10 5 100 100 5
AllocationParam 250 250 0.25 30 1 2
trackingCfg 1 2 250 20 52 82 50 90
sensorStart

是否可以添加一个

chirpCfg 2 2 0 0 0 0 0 2

以使得三根天线全部使能。

我进行了以上的操作,然后看到CCS报错如下

我想问一下是否有办法使得这个demo能够使能3根天线正常工作。