This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

HDC1080: hdc1080 数据转换时间的问题。

Part Number: HDC1080


1、项目使用高度集成库,无法提供延时时间,请问是否有什么方法能不用此延时。比如说向某个寄存器写入数据开始采集数据并转换。

 读取ID均正常。

 读取温度和湿度全为FF.

  • 您好,读取温度和湿度这里,主机重新发送restart命令之后,地址为0x81之后没有收到ACK信号,所以后面读取的寄存器的值都是FF。

    但是上面读取ID的时序是没问题的,0x81之后能正确收到ACK信号。

    下面读取温度和湿度的时序是没问题的,符合读时序的要求,原因在于第九个clock这里没有将SCL拉低。