This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

FDC2114EVM: 可否用来测量pF级电容的变化?

Part Number: FDC2114EVM


1.FDC2114EVM是否可以用来测量pF级电容的连续变化,并将数据采集下来进一步演示?

2.FDC2114EVM是否需要自己编程?

  • .FDC2114EVM是否可以用来测量pF级电容的连续变化,并将数据采集下来进一步演示?

    FDC2114EVM 有18uH的电感, 因此,电容推荐值再33pF左右,这将使系统对电容变化更加敏感。

    .FDC2114EVM是否需要自己编程?

    通过EVM GUI加载固件。可直接参考EVM user's guide中的步骤。