This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

IWR6843ISK: iwr6843isk

Part Number: IWR6843ISK


工程师您好,我使用的SDK版本是3.5 用的demo是out of box 通过串口解析数据 我看了手册说是可以配置雷达输出的内容 understanding_oob_uart_data.html ,我目前想要点的坐标 速度和角度信息 该如何配置?

  • mmwave demo visualizer GUI里有Record按钮可以保存串口输出数据,然后可以参考C:\ti\mmwave_sdk_03_05_00_04\packages\ti\demo\parser_scripts解析代码。具体可以参考mmwave_sdk_user_guide.pdf文档。
    The saving of data can be manually stopped using the "Record Stop" button (if the max limits are not reached). Sample python scripts to parse the point cloud output of the demo are provided in mmwave_sdk_\packages\ti\demo\parser_scripts. mmw_demo_example_scr ipt.py is the top level example script that uses the parser module provided in parser_mmw_demo.py. User can customize the mmw_demo_example_script.py to parse their captured files and process it as per their requirements

  • 工程师,你好,我的意思是如何配置雷达发送的cfg文件如何修改 ,才能使雷达从串口输出的数据包含坐标,角度,速度

  • mmw demo输出的数据已经包含了坐标信息,速度信息,请看一下下面文档里的Coordinate Geometry
    C:/ti/mmwave_sdk_03_05_00_04/packages/ti/demo/xwr68xx/mmw/docs/doxygen/html/index.html