This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LDC1614: 关于自校正、振荡波形、错误标志位、寄存器配置、IIC通讯相关问题。

Part Number: LDC1614


1、在相同的软硬件条件下,我将AUTO_AMP_DIS和RP_OVERRIDE_EN置0,传感器可以正常工作,但是DRIVE_CURRENT1的值与我所写给它的值不同。我记下此刻所读取到的DRIVE_CURRENT1的值,把AUTO_AMP_DIS和RP_OVERRIDE_EN置1,并将刚刚记下的值在传感器上电后写给DRIVE_CURRENT1,此时读取到Channel 1 Conversion Amplitude Error Flag。我使用的IDRIVE1计算公式:IDRIVE1 = (3.14*(3.3/2)*1000000)/(4*谐振阻抗)。想问下自校正除了校正电流以外还会调整传感器的其他地方么?使能/禁止自校正时DRIVE_CURRENT1的值相同,为什么还会出现转换不了的情况?什么时候才会触发振幅转换错误?INT_IDRIVE1该如何配置?

2、下图中蓝色和绿色分别为电容两边信号,紫色为蓝色减绿色信号,请问下图波形是否正常,如果不正常是什么原因,应该如何修改?

===========================该问题对应的线圈参数及寄存器配置================================

寄存器配置:

//第二版电路                RCOUNT OFFSET SETCNT CLKDVI DRVCUR
int16_t CH1_Para[5] = {0xD3C5, 0x0000, 0x0023, 0x1001, 0x7000};
//                                ERRCFG MUXCFG CONFIG
int16_t CHx_Para[3] = {0xF801, 0x420D, 0x5C81};

下图为该线圈的设计参数: