This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: 与PC链接距离较远,使用USB延长线无法识别usb接口问题如何解决

Part Number: DCA1000EVM
Other Parts Discussed in Thread: IWR1443,

我需要IWR1443+DCA1000EVM距离地面10米高处放置进行使用,而PC端在地面放置,因此需要加长的usb线进行控制,但是,目前DCA1000EVM使用加长的usb数据线进行控制Windows无法识别,线太长了,一米的usb线可以使用,请问pc端和采集板距离10米,该如何实现采集呢?

1.USB延长线最长多少米可以识别到usb端口并使用进行控制?

2.是否可以用采集板端将micro usb转网线,网线10米,然后网线再转回usb到pc端实现控制?

3.或者有什么其他办法?