This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMP275: TMP275多次点测,温度不变

Part Number: TMP275


用TMP275读外部环境温度,每次IIC读出来的2个Byte的波形都一样,是一个正常的温度值25.238℃,有配置分辨率为0.0625℃,之前用TMP275作为基准测温芯片用于FT量产是ok的,近期莫名其妙出现温度不变的情况,请大佬看看有什么原因。

  • 您好,

    所测环境温度是否改变了?不同的分辨率转换时间是不同的,0.0625℃分辨率转换时间典型值是220ms,您是否间隔一个转换时间去读取转换结果?

  • 您好!

    275data转换时间是充足的,现在我想确认下VCC在2.7V~5.5V宽电压域供电时对测量精度的影响,现在我司是需要用275芯片在常温环境下对我司的芯片进行温度校准,使得校准后的芯片精度在±0.5℃范围内,所以275作为基准测温芯片,自身的精度有要求,需要在测量时能达到0.0625℃的分辨率,±0.5℃的精度,我看datasheet上只描述了3V~5.5V的精度和分辨率,而芯片的工作电压在2.7V~5.5V,对于2.7V~3V的这部分没有描述,而根据我自身的验证结果,我需要降VCC降到2.9V才能读到变化的温度,请问这一现象是否正常,还有我IIC的协议配置如下:0x9e----0x01----0x60----0x9e----0x00---0x9f---Byte---Byte。

  • 而根据我自身的验证结果,我需要降VCC降到2.9V才能读到变化的温度,请问这一现象是否正常,

    您的意思是VCC供电电压需要2.7V升到2.9V才能读到变化的温度?供电电压2.9V以下读不到?

  • 5V和3.3V,3V试过,不行,所以我降到了2.9V发现可以更新了,所以我现在想了解供电电压和外部环境温度对测量精度的影响,我需要施加怎样的条件才可以使275具有±0.5℃的测量精度。

  • 如下datasheet截图,在3.3V供电时,测温范围是–20°C to 100°C时,测量精度最大是±0.5℃

    您是怎样保证在5V、3.3V、3V和2.9V供电电压时测试环境温度一样的?

    我想找的温度误差与供电电压纹波噪声方面的参数PSRR,但是我没有找到(这个传感器比较老了,一些资料可能都丢失了)。我想这可能也与供电电压的质量有关,根据经验PSRR参数会随着供电纹波噪声的频率升高而降低的。我想您也可以从供电电压的质量方面找找原因。