用TMP275读外部环境温度,每次IIC读出来的2个Byte的波形都一样,是一个正常的温度值25.238℃,有配置分辨率为0.0625℃,之前用TMP275作为基准测温芯片用于FT量产是ok的,近期莫名其妙出现温度不变的情况,请大佬看看有什么原因。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好!
275data转换时间是充足的,现在我想确认下VCC在2.7V~5.5V宽电压域供电时对测量精度的影响,现在我司是需要用275芯片在常温环境下对我司的芯片进行温度校准,使得校准后的芯片精度在±0.5℃范围内,所以275作为基准测温芯片,自身的精度有要求,需要在测量时能达到0.0625℃的分辨率,±0.5℃的精度,我看datasheet上只描述了3V~5.5V的精度和分辨率,而芯片的工作电压在2.7V~5.5V,对于2.7V~3V的这部分没有描述,而根据我自身的验证结果,我需要降VCC降到2.9V才能读到变化的温度,请问这一现象是否正常,还有我IIC的协议配置如下:0x9e----0x01----0x60----0x9e----0x00---0x9f---Byte---Byte。