Other Parts Discussed in Thread: LMT70, TMP117
最近在做一个气体检测的装置,用到的CO和H2S传感器 三电平的 传感器电路用的TI官方推荐的典型电路,在-20°低温下,91000输出的响应速度和值与常温(20°)差距很大,请问怎么处理?如果需要低温补偿?应该怎么补偿
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
下面用户帖子的问题与您的问题类似,请查看帖子回复:
帖子回复大体意思是:
您可以使用LMP91000 内部集成的温度传感器用于本地温度测量,然后将其用于主控端正在处理的传感器补偿计算。如果内部集成的温度传感器精度参数不满足应用需求,您也可以选择使用高精度外部温度传感器,如TMP117 (数字)或LMT70 (模拟)直接与您的主控端连接。
您所使用的传感器的制造商应该能够向您提供如何利用温度进行补偿的信息。例如,LMP91000支持的传感器之一是Alphasense提供的A2-02传感器-它们提供此文档
http://www.alphasense.com/WEB1213/wp-content/uploads/2013/07/AAN_005.pdf
另一个示例是来自Spec Sensors的文档,该文档讨论了相同的主题,其中包含五个传感器,LMP91000也支持这些传感器
http://www.spec-sensors.com/wp-content/uploads/2016/06/SPEC-AN-104-Environmental-Effects.pdf