This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: AWR2243多片级联雷达MIMO时TX发射控制程序

Part Number: AWR2243


请问,在用AWR2243设计两片或者四片级联雷达,采用MIMO制式,比如设计两片级联雷达,主芯片TX1、TX2、TX3,从芯片TX4、TX5、TX6.

若按照TX6到TX1次序轮流等间隔时间发射,每帧轮询发射N次。看到资料说主芯片采用软件触发,从芯片采用硬件SYNC_IN触发。

程序里设置主芯片SYNC_OUT发射信号,经过buffer到主从芯片SYNC_IN引脚,那么从芯片就可以TX6---TX4发射,然后轮到主芯片TX发射,这时的主芯片发射是跳转到软件触发吗?

从芯片的TX4与主芯片的TX3之间的chirp间隔是怎么实现控制的?

或者是主从芯片都是采用SYNC_IN触发的?