你好:
请问,TMAG5170 寄存器配置有先后顺序吗?另外,DATA_TYPE 一直写不进去,别的寄存器是可以的,请问是什么原因?谢谢!!!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
寄存器配置没有先后顺序要求
DATA_TYPE 一直写不进去,别的寄存器是可以的
仅这3bits写不进去是吗? SYSTEM_CONFIG寄存器的其他bits可以写入是吗?写不进去是指写入非0值后,读出仍为000?您可以用示波器或逻辑分析仪抓取写入这个寄存器的SPI时序图吗,然后附在这里?

在TMAG5170产品首页提供了 C code example,不知道您是否已经下载参考?
TMAG5170产品首页链接:https://www.ti.com.cn/product/cn/TMAG5170

SENSOR_CONFIG Register配置后可以正确读出来是吗?
另外,32 bits SPI帧的低4位是CRC位,启用CRC后,如果未收到正确的CRC代码,设备将忽略SDI命令。因此请检查SDI写入帧是否存在CRC错误。CRC代码由多项式x^4 + x + 1生成,初始CRC位是b1111。具体见 datasheet 7.5.2.5 SPI CRC章节。
要在SDI禁用CRC,请发送SPI SDI命令x0F000407。

仔细阅读 datasheet 7.5.2.6 SPI Frame部分,我发现只有在regular read模式下,也就是 DATA_TYPE = 000b时才能读取寄存器值,在DATA_TYPE > 000b时,SDO输出的是 DATA_TYPE寄存器位定义的两通道数据,如下截图部分所示。因此DATA_TYPE配置非0值后,就不能读取寄存器值了。